How to verify whether the DDRAM connected to imx6 processor , is in self refresh mode ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to verify whether the DDRAM connected to imx6 processor , is in self refresh mode ?

998件の閲覧回数
prakeerthi_y
Contributor I

In free-scale solo board,2 DDR RAMs placed in the board. While optimizing power , we tried to test to put the DDR into self refreshing mode. But I cant create a scenario ,where I can see the self-refresh mode enabled bit in MMDC Control and status register (25 bit) ..Need assistance in how to test the working of self refresh mode..

Thank you.

ラベル(4)
0 件の賞賛
返信
1 返信

926件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi prakeerthi

there is no one bit settings and entering self-refresh mode is performed

during procedure described in sect.44.4.6.2 Self refresh and Frequency change

entry/exit i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

One can check with oscilloscope signals described here.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信