How to using ecspi2 and ecspi3 to the M4 processor in i.MX8MQ6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to using ecspi2 and ecspi3 to the M4 processor in i.MX8MQ6?

731 次查看
kerazus
Contributor II

Hi,

 

When we performed the operations in the attached document on the M4 processor of the IMX8MQ, we were unable to use the BT_UART4 pins (J2.20, 22, 24, 26) as ECSPI2. However, we were able to use and control the pins (J2.20, 22, 24, 26) as GPIO. Can you help us to enable ECSPI2 on the M4 processor? (Note: I using evk DART-MX8M.)

imxbt_uart4.PNG


Below I share the sample code written in ecspi2. When used below code, ecspi2 could'nt work but the same pins I could use it as an GPIO pin. Do I need to changed dts files for using to ecspi2/ecspi3.


#define ECSPI_TRANSFER_SIZE     64

#define ECSPI_TRANSFER_BAUDRATE 500000U

#define ECSPI_MASTER_BASEADDR   ECSPI2

#define ECSPI_MASTER_CLK_FREQ                                                                \

    CLOCK_GetPllFreq(kCLOCK_SystemPll1Ctrl) / (CLOCK_GetRootPreDivider(kCLOCK_RootEcspi2)) / \

        (CLOCK_GetRootPostDivider(kCLOCK_RootEcspi2))

#define ECSPI_MASTER_TRANSFER_CHANNEL kECSPI_Channel0

    ecspi_transfer_t masterXfer;

    ecspi_master_config_t masterConfig;

    uint32_t masterRxData[ECSPI_TRANSFER_SIZE] = {0};

    uint32_t masterTxData[ECSPI_TRANSFER_SIZE] = {0};

 

    CLOCK_SetRootMux(kCLOCK_RootEcspi2, kCLOCK_EcspiRootmuxSysPll1); /* Set ECSPI1 source to SYSTEM PLL1 800MHZ */

    CLOCK_SetRootDivider(kCLOCK_RootEcspi2, 2U, 5U);                 /* Set root clock to 800MHZ / 10 = 80MHZ */

 

    ECSPI_MasterGetDefaultConfig(&masterConfig);

    masterConfig.baudRate_Bps   = ECSPI_TRANSFER_BAUDRATE;

    masterConfig.enableLoopback = true;

    ECSPI_MasterInit(ECSPI_MASTER_BASEADDR, &masterConfig, ECSPI_MASTER_CLK_FREQ);

 

    masterXfer.txData   = masterTxData;

    masterXfer.rxData   = masterRxData;

    masterXfer.dataSize = ECSPI_TRANSFER_SIZE;

    masterXfer.channel  = ECSPI_MASTER_TRANSFER_CHANNEL;

 

    GPIO_PinWrite(BT_GPIO, BT_GPIO_PIN, 1U);

    ECSPI_MasterTransferBlocking(ECSPI_MASTER_BASEADDR, &masterXfer);

    GPIO_PinWrite(BT_GPIO, BT_GPIO_PIN, 0U);

0 项奖励
回复
1 回复

711 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @kerazus!

Thank you for contacting NXP Support!

 

You should configure the RDC for use it under M core.

 

The configuration can be done on BL31:

 

https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mq/imx8mq_bl31_setup.c

 

https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQRM

 

Best Regards!

Chavira

0 项奖励
回复