How to use wifi module with usdhc1 on imx8mp-evk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use wifi module with usdhc1 on imx8mp-evk board

2,355件の閲覧回数
dskim2
Contributor IV

Dear

I want to bring up Wifi module by using SD/MMC (SDIO interface, use USDHC1 slot).

There is no usdhc1 part in the original kernel dts file.

So I have tried to change "imx8mm-evk.dts" of kernel but it seem is not work.

Attached file is modified file.(imx8mp-evk.dts).

Please check.

Best Regards

 

0 件の賞賛
返信
3 返答(返信)

2,332件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Have you check the signals and voltage on your wifi module? Could you tell me which wifi module are you using?

Which version of BSP are you using?

Could you describe more about how it is not working?

How you loading the wifi driver and the firmware?

Is there any error message when the board boot up?

0 件の賞賛
返信

2,326件の閲覧回数
dskim2
Contributor IV

Hi

I builed Yocto version 6.1.22_2.0.0

Looking at the imx8mp.dtsi file, there is a usdhc1: mmc@30b40000 part, but the mmc@30b40000 part is not displayed when booting, and ifconfig mlan0 up is performed, ifconfig: SIOCGIFFLAGS: No such device is displayed.

 

below is the device booting log

 


U-Boot SPL 2023.04-lf_v2023.04+gaf7d004eaf (Jun 06 2023 - 14:59:40 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x0, pagesize 0x200, ivt offset 0x0
NOTICE: Do not release JR0 to NS as it can be used by HAB
NOTICE: BL31: v2.8(release):android-13.0.0_2.0.0-0-ge4b2dbfa5
NOTICE: BL31: Built : 06:14:17, Jun 2 2023


U-Boot 2023.04-lf_v2023.04+gaf7d004eaf (Jun 06 2023 - 14:59:40 +0000)

CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 76C
Reset cause: POR
Model: NXP i.MX8MPlus LPDDR4 EVK board
DRAM: 2 GiB
tcpc_init: Can't find bus
setup_typec: tcpc port2 init failed, err=-22
setup_pd_switch: Can't find device id=0x72
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
Core: 240 devices, 30 uclasses, devicetree: separate
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Fail to setup video link
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
switch to partitions #0, OK
mmc2(part 0) is current device
flash target is MMC:2
Net:
Warning: ethernet@30bf0000 (eth1) using random MAC address - 26:3f:12:cd:4b:14

Warning: ethernet@30be0000 (eth0) using random MAC address - 9a:05:da:d4:c6:60
eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 2 1 0
Working FDT set to 43000000
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
starting USB...
Bus usb@38100000: Failed to initialize board for imx8m USB
probe failed, error -1
Bus usb@38200000: Register 2000140 NbrPorts 2
Starting the controller
USB XHCI 1.10
scanning bus usb@38200000 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
MMC: no card present
switch to partitions #0, OK
mmc2(part 0) is current device
Scanning mmc 2:1...
87557 bytes read in 5 ms (16.7 MiB/s)
Working FDT set to 43000000
MMC: no card present
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
switch to partitions #0, OK
mmc2(part 0) is current device
Failed to load 'boot.scr'
32121344 bytes read in 96 ms (319.1 MiB/s)
Booting from mmc ...
87557 bytes read in 9 ms (9.3 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Working FDT set to 43000000
clk usb_phy_root_clk already disabled
Using Device Tree in place at 0000000043000000, end 0000000043018604
Working FDT set to 43000000

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.1.22+g66e442bc7fdc (oe-user@oe-host) (aarch64-pok
y-linux-gcc (GCC) 12.2.0, GNU ld (GNU Binutils) 2.40.20230119) #1 SMP PREEMPT Mo
n Jun 12 12:31:27 UTC 2023
[ 0.000000] Machine model: NXP i.MX8MPlus EVK board
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma':
size 960 MiB
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000094300000, s
ize 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0buffer@94300000, compatib
le id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bfffffff
]
[ 0.000000] NUMA: NODE_DATA [mem 0xbfbb3700-0xbfbb5fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x0000000055ffffff]
[ 0.000000] node 0: [mem 0x0000000058000000-0x00000000923fffff]
[ 0.000000] node 0: [mem 0x0000000092400000-0x00000000943fffff]
[ 0.000000] node 0: [mem 0x0000000094400000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges
[ 0.000000] cma: Reserved 32 MiB at 0x00000000bba00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s44520 r8192 d29208 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507904
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk2p2 r
ootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes,
linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes,
linear)
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] Memory: 1926136K/2064384K available (19584K kernel code, 1608K rw
data, 6708K rodata, 3328K init, 644K bss, 105480K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jif
fies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 160 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles:
0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 21990
23255500ns
[ 0.000565] Console: colour dummy device 80x25
[ 0.000623] Calibrating delay loop (skipped), value calculated using timer fr
equency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000633] pid_max: default: 32768 minimum: 301
[ 0.000689] LSM: Security Framework initializing
[ 0.000769] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, line
ar)
[ 0.000780] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes,
linear)
[ 0.002070] cblist_init_generic: Setting adjustable number of callback queues
.
[ 0.002081] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.002151] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.002308] rcu: Hierarchical SRCU implementation.
[ 0.002311] rcu: Max phase no-delay instances is 1000.
[ 0.004147] EFI services will not be available.
[ 0.004387] smp: Bringing up secondary CPUs ...
[ 0.004830] Detected VIPT I-cache on CPU1
[ 0.004913] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.004948] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.005441] Detected VIPT I-cache on CPU2
[ 0.005498] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.005519] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.005951] Detected VIPT I-cache on CPU3
[ 0.006010] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.006028] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.006083] smp: Brought up 1 node, 4 CPUs
[ 0.006089] SMP: Total of 4 processors activated.
[ 0.006093] CPU features: detected: 32-bit EL0 Support
[ 0.006096] CPU features: detected: 32-bit EL1 Support
[ 0.006100] CPU features: detected: CRC32 instructions
[ 0.006153] CPU: All CPU(s) started at EL2
[ 0.006170] alternatives: applying system-wide alternatives
[ 0.007736] devtmpfs: initialized
[ 0.018435] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma
x_idle_ns: 7645041785100000 ns
[ 0.018456] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.019421] pinctrl core: initialized pinctrl subsystem
[ 0.022628] DMI not present or invalid.
[ 0.023206] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.024222] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.024468] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allo
cations
[ 0.024647] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic al
locations
[ 0.024699] audit: initializing netlink subsys (disabled)
[ 0.024817] audit: type=2000 audit(0.020:1): state=initialized audit_enabled=
0 res=1
[ 0.025295] thermal_sys: Registered thermal governor 'step_wise'
[ 0.025299] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.025328] cpuidle: using governor menu
[ 0.025520] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.025601] ASID allocator initialised with 65536 entries
[ 0.026954] Serial: AMBA PL011 UART driver
[ 0.027022] imx mu driver is registered.
[ 0.027042] imx rpmsg driver is registered.
[ 0.039002] imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.047705] platform 32e60000.mipi_dsi: Fixed dependency cycle(s) with /soc@0
/bus@30800000/i2c@30a30000/adv7535@3d
[ 0.047738] platform 32e60000.mipi_dsi: Fixed dependency cycle(s) with /soc@0
/bus@32c00000/lcd-controller@32e80000
[ 0.048177] platform 32e90000.lcd-controller: Fixed dependency cycle(s) with
/soc@0/bus@32c00000/ldb@32ec005c
[ 0.049416] platform 32c00000.bus:ldb@32ec005c: Fixed dependency cycle(s) wit
h /soc@0/bus@30800000/i2c@30a30000/lvds-to-hdmi-bridge@4c
[ 0.050884] platform 32e40000.csi: Fixed dependency cycle(s) with /soc@0/bus@
30800000/i2c@30a30000/ov5640_mipi@3c
[ 0.054475] platform 32fc6000.lcd-controller: Fixed dependency cycle(s) with
/soc@0/bus@30c00000/hdmi@32fd8000
[ 0.061876] platform cbtl04gp: Fixed dependency cycle(s) with /soc@0/bus@3080
0000/i2c@30a30000/tcpc@50/connector
[ 0.062441] KASLR disabled due to lack of seed
[ 0.081243] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.081252] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.081257] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.081260] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.081264] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.081268] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.081274] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.081279] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.083324] ACPI: Interpreter disabled.
[ 0.084094] iommu: Default domain type: Translated
[ 0.084099] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.084369] SCSI subsystem initialized
[ 0.084673] usbcore: registered new interface driver usbfs
[ 0.084704] usbcore: registered new interface driver hub
[ 0.084728] usbcore: registered new device driver usb
[ 0.086094] mc: Linux media interface: v0.10
[ 0.086127] videodev: Linux video capture interface: v2.00
[ 0.086204] pps_core: LinuxPPS API ver. 1 registered
[ 0.086208] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome
tti <giometti@linux.it>
[ 0.086219] PTP clock support registered
[ 0.086399] EDAC MC: Ver: 3.0.0
[ 0.087577] FPGA manager framework
[ 0.087660] Advanced Linux Sound Architecture Driver Initialized.
[ 0.088177] Bluetooth: Core ver 2.22
[ 0.088204] NET: Registered PF_BLUETOOTH protocol family
[ 0.088207] Bluetooth: HCI device and connection manager initialized
[ 0.088214] Bluetooth: HCI socket layer initialized
[ 0.088219] Bluetooth: L2CAP socket layer initialized
[ 0.088229] Bluetooth: SCO socket layer initialized
[ 0.088584] vgaarb: loaded
[ 0.089073] clocksource: Switched to clocksource arch_sys_counter
[ 0.089253] VFS: Disk quotas dquot_6.6.0
[ 0.089291] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.089444] pnp: PnP ACPI: disabled
[ 0.096222] NET: Registered PF_INET protocol family
[ 0.096372] IP idents hash table entries: 32768 (order: 6, 262144 bytes, line
ar)
[ 0.097907] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 1638
4 bytes, linear)
[ 0.097957] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes,
linear)
[ 0.097972] TCP established hash table entries: 16384 (order: 5, 131072 bytes
, linear)
[ 0.098083] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linea
r)
[ 0.098512] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.098596] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.098642] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.098791] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.099124] RPC: Registered named UNIX socket transport module.
[ 0.099128] RPC: Registered udp transport module.
[ 0.099131] RPC: Registered tcp transport module.
[ 0.099133] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.099850] PCI: CLS 0 bytes, default 64
[ 0.100488] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counte
rs available
[ 0.101608] kvm [1]: IPA Size Limit: 40 bits
[ 0.103225] kvm [1]: GICv3: no GICV resource entry
[ 0.103229] kvm [1]: disabling GICv2 emulation
[ 0.103238] kvm [1]: GIC system register CPU interface enabled
[ 0.103320] kvm [1]: vgic interrupt IRQ9
[ 0.103403] kvm [1]: Hyp mode initialized successfully
[ 0.104545] Initialise system trusted keyrings
[ 0.104701] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.111101] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.111694] NFS: Registering the id_resolver key type
[ 0.111719] Key type id_resolver registered
[ 0.111722] Key type id_legacy registered
[ 0.111797] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.111802] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering
...
[ 0.111822] jffs2: version 2.2. (NAND) 짤 2001-2006 Red Hat, Inc.
[ 0.112137] 9p: Installing v9fs 9p2000 file system support
[ 0.148367] Key type asymmetric registered
[ 0.148372] Asymmetric key parser 'x509' registered
[ 0.148411] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2
43)
[ 0.148417] io scheduler mq-deadline registered
[ 0.148421] io scheduler kyber registered
[ 0.156527] EINJ: ACPI disabled.
[ 0.168224] imx-sdma 30bd0000.dma-controller: Direct firmware load for imx/sd
ma/sdma-imx7d.bin failed with error -2
[ 0.168237] imx-sdma 30bd0000.dma-controller: Falling back to sysfs fallback
for: imx/sdma/sdma-imx7d.bin
[ 0.169941] mxs-dma 33000000.dma-apbh: initialized
[ 0.177125] SoC: i.MX8MP revision 1.1
[ 0.181283] Bus freq driver module loaded
[ 0.187640] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.190477] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 17, base_baud
= 5000000) is a IMX
[ 0.190604] serial serial0: tty port ttymxc0 registered
[ 0.190944] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 18, base_baud
= 5000000) is a IMX
[ 0.191450] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 19, base_baud
= 1500000) is a IMX
[ 1.384193] printk: console [ttymxc1] enabled
[ 1.411125] loop: module loaded
[ 1.416038] megasas: 07.719.03.00-rc1
[ 1.426072] spi-nor spi0.0: n25q256ax1 (32768 Kbytes)
[ 1.435890] tun: Universal TUN/TAP device driver, 1.6
[ 1.442256] thunder_xcv, ver 1.0
[ 1.445534] thunder_bgx, ver 1.0
[ 1.448794] nicpf, ver 1.0
[ 1.454358] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - versio
n
[ 1.461595] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.466968] hclge is initializing
[ 1.470306] e1000: Intel(R) PRO/1000 Network Driver
[ 1.475192] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.480979] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.485948] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.491907] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.497347] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.502959] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.509233] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.515399] sky2: driver version 1.30
[ 1.519878] usbcore: registered new interface driver r8152
[ 1.525651] VFIO - User Level meta-driver version: 0.3
[ 1.532831] platform 38100000.usb: Fixed dependency cycle(s) with /soc@0/bus@
30800000/i2c@30a30000/tcpc@50
[ 1.548638] usbcore: registered new interface driver uas
[ 1.554023] usbcore: registered new interface driver usb-storage
[ 1.560098] usbcore: registered new interface driver usbserial_generic
[ 1.566661] usbserial: USB Serial support registered for generic
[ 1.572704] usbcore: registered new interface driver ftdi_sio
[ 1.578471] usbserial: USB Serial support registered for FTDI USB Serial Devi
ce
[ 1.585813] usbcore: registered new interface driver usb_serial_simple
[ 1.592361] usbserial: USB Serial support registered for carelink
[ 1.598472] usbserial: USB Serial support registered for zio
[ 1.604156] usbserial: USB Serial support registered for funsoft
[ 1.610180] usbserial: USB Serial support registered for flashloader
[ 1.616555] usbserial: USB Serial support registered for google
[ 1.622498] usbserial: USB Serial support registered for libtransistor
[ 1.629045] usbserial: USB Serial support registered for vivopay
[ 1.635072] usbserial: USB Serial support registered for moto_modem
[ 1.641358] usbserial: USB Serial support registered for motorola_tetra
[ 1.647991] usbserial: USB Serial support registered for nokia
[ 1.653844] usbserial: USB Serial support registered for novatel_gps
[ 1.660219] usbserial: USB Serial support registered for hp4x
[ 1.665985] usbserial: USB Serial support registered for suunto
[ 1.671924] usbserial: USB Serial support registered for siemens_mpi
[ 1.678312] usbcore: registered new interface driver usb_ehset_test
[ 1.688347] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/300
00000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.703227] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.709443] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-
01-01T00:00:00 UTC (0)
[ 1.718691] i2c_dev: i2c /dev entries driver
[ 1.728986] Bluetooth: HCI UART driver ver 2.3
[ 1.733457] Bluetooth: HCI UART protocol H4 registered
[ 1.738604] Bluetooth: HCI UART protocol BCSP registered
[ 1.743948] Bluetooth: HCI UART protocol LL registered
[ 1.749097] Bluetooth: HCI UART protocol ATH3K registered
[ 1.754518] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.760914] Bluetooth: HCI UART protocol Broadcom registered
[ 1.766601] Bluetooth: HCI UART protocol QCA registered
[ 1.772054] EDAC MC: ECC not enabled
[ 1.777289] sdhci: Secure Digital Host Controller Interface driver
[ 1.783483] sdhci: Copyright(c) Pierre Ossman
[ 1.788874] Synopsys Designware Multimedia Card Interface Driver
[ 1.795837] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.804899] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.811960] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.818913] usbcore: registered new interface driver usbhid
[ 1.824497] usbhid: USB HID core driver
[ 1.828945] mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using
dummy regulator
[ 1.834934] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 1.837887] : mipi_csis_imx8mp_phy_reset, No remote pad found!
[ 1.850356] mxc-mipi-csi2-sam 32e40000.csi: lanes: 2, hs_settle: 13, clk_sett
le: 2, wclk: 1, freq: 500000000
[ 1.862404] mxc-isi 32e00000.isi: mxc_isi.0 registered successfully
[ 1.875101] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.883581] optee: probing for conduit method.
[ 1.888064] optee: revision 3.21 (1962aec9)
[ 1.888634] optee: dynamic shared memory is enabled
[ 1.898041] optee: initialized driver
[ 1.904896] Galcore version 6.4.11.p1.658245
[ 1.926357] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 1.927459] [drm] Initialized vivante 1.0.0 20170808 for 40000000.mix_gpu_ml
on minor 0
[ 1.933953] mmcblk2: mmc2:0001 DG4016 14.7 GiB
[ 1.942653] hantrodec 0 : module inserted. Major = 510
[ 1.947932] mmcblk2: p1 p2 p3
[ 1.951119] hantrodec 1 : module inserted. Major = 510
[ 1.955914] mmcblk2boot0: mmc2:0001 DG4016 4.00 MiB
[ 1.960652] hantroenc: HW at base <0000000038320000> with ID <0x80006200>
[ 1.964900] mmcblk2boot1: mmc2:0001 DG4016 4.00 MiB
[ 1.970554] hx280enc: module inserted. Major <509>
[ 1.977171] mmcblk2rpmb: mmc2:0001 DG4016 4.00 MiB, chardev (234:0)
[ 1.986192] NET: Registered PF_LLC protocol family
[ 1.992687] NET: Registered PF_INET6 protocol family
[ 1.999149] Segment Routing with IPv6
[ 2.002865] In-situ OAM (IOAM) with IPv6
[ 2.006840] NET: Registered PF_PACKET protocol family
[ 2.011937] bridge: filtering via arp/ip/ip6tables is no longer available by
default. Update your scripts to load br_netfilter if you need this.
[ 2.025902] Bluetooth: RFCOMM TTY layer initialized
[ 2.030815] Bluetooth: RFCOMM socket layer initialized
[ 2.035995] Bluetooth: RFCOMM ver 1.11
[ 2.039758] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.045077] Bluetooth: BNEP filters: protocol multicast
[ 2.050311] Bluetooth: BNEP socket layer initialized
[ 2.055281] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.061207] Bluetooth: HIDP socket layer initialized
[ 2.067220] 8021q: 802.1Q VLAN Support v1.8
[ 2.071434] lib80211: common routines for IEEE802.11 drivers
[ 2.077211] 9pnet: Installing 9P2000 support
[ 2.081607] Key type dns_resolver registered
[ 2.086853] registered taskstats version 1
[ 2.090983] Loading compiled-in X.509 certificates
[ 2.152733] nxp-pca9450 0-0025: pca9450bc probed.
[ 2.157556] i2c i2c-0: IMX I2C adapter registered
[ 2.163581] adv7511 1-003d: supply avdd not found, using dummy regulator
[ 2.170397] adv7511 1-003d: supply dvdd not found, using dummy regulator
[ 2.177146] adv7511 1-003d: supply pvdd not found, using dummy regulator
[ 2.183893] adv7511 1-003d: supply a2vdd not found, using dummy regulator
[ 2.190720] adv7511 1-003d: supply v3p3 not found, using dummy regulator
[ 2.197461] adv7511 1-003d: supply v1p2 not found, using dummy regulator
[ 2.205633] adv7511 1-003d: Probe failed. Remote port 'mipi_dsi@32e60000' dis
abled
[ 2.268132] it6263 1-004c: Probe failed. Remote port 'lvds-channel@0' disable
d
[ 2.276092] ov5640 1-003c: supply DOVDD not found, using dummy regulator
[ 2.282915] ov5640 1-003c: supply AVDD not found, using dummy regulator
[ 2.289571] ov5640 1-003c: supply DVDD not found, using dummy regulator
[ 2.343627] ov5640 1-003c: ov5640_read_reg: error: reg=300a
[ 2.349216] ov5640 1-003c: ov5640_check_chip_id: failed to read chip identifi
er
[ 2.360341] i2c i2c-1: IMX I2C adapter registered
[ 2.366906] pca953x 2-0020: supply vcc not found, using dummy regulator
[ 2.373637] pca953x 2-0020: using no AI
[ 2.377743] pca953x 2-0020: failed writing register
[ 2.382890] i2c i2c-2: IMX I2C adapter registered
[ 2.388660] imx8mp-ldb 32c00000.bus:ldb@32ec005c: Failed to create device lin
k (0x180) with 32c00000.bus:phy@32ec0128
[ 2.399619] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dum
my regulator
[ 2.408239] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dum
my regulator
[ 2.419106] pwm-backlight lvds_backlight: supply power not found, using dummy
regulator
[ 2.420017] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges
:
[ 2.434416] imx6q-pcie 33800000.pcie: IO 0x001ff80000..0x001ff8ffff ->
0x0000000000
[ 2.442638] imx6q-pcie 33800000.pcie: MEM 0x0018000000..0x001fefffff ->
0x0018000000
[ 2.445584] dwhdmi-imx 32fd8000.hdmi: Detected HDMI TX controller v2.13a with
HDCP (samsung_dw_hdmi_phy2)
[ 2.463020] dwhdmi-imx 32fd8000.hdmi: registered DesignWare HDMI I2C bus driv
er
[ 2.472148] phy phy-32f00000.pcie-phy.4: phy poweron failed --> -110
[ 2.476148] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_
crtc_ops)
[ 2.478533] imx6q-pcie 33800000.pcie: waiting for PHY ready timeout!
[ 2.486484] imx-drm display-subsystem: bound imx-lcdifv3-crtc.1 (ops lcdifv3_
crtc_ops)
[ 2.492864] imx6q-pcie: probe of 33800000.pcie failed with error -110
[ 2.500762] imx-drm display-subsystem: bound imx-lcdifv3-crtc.2 (ops lcdifv3_
crtc_ops)
[ 2.515232] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[ 2.522271] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bu
s@32c00000/mipi_dsi@32e60000 to encoder DSI-40: -19
[ 2.533871] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e6
0000.mipi_dsi
[ 2.542147] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridg
e: -19
[ 2.549826] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_d
sim_ops)
[ 2.557738] imx-drm display-subsystem: bound 32c00000.bus:ldb@32ec005c (ops i
mx8mp_ldb_ops)
[ 2.566136] imx-drm display-subsystem: bound 32fd8000.hdmi (ops dw_hdmi_imx_o
ps)
[ 2.574488] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on
minor 1
[ 2.582395] imx-drm display-subsystem: [drm] Cannot find any crtc or sizes
[ 2.594788] pps pps0: new PPS source ptp0
[ 2.710226] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.717273] imx-dwmac 30bf0000.ethernet: IRQ eth_lpi not found
[ 2.724041] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51
[ 2.730849] imx-dwmac 30bf0000.ethernet: DWMAC4/5
[ 2.735653] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported
[ 2.742800] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported
[ 2.749947] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported
[ 2.756096] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog
Timer
[ 2.763760] imx-dwmac 30bf0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 2.770558] imx-dwmac 30bf0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 2.777370] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off
=256)
[ 2.784954] imx-dwmac 30bf0000.ethernet: Using 34/40 bits DMA host/device wid
th
[ 2.993740] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 2.999272] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus nu
mber 1
[ 3.007324] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220fe6d hci version 0x110
quirks 0x0000002001010010
[ 3.016769] xhci-hcd xhci-hcd.1.auto: irq 224, io mem 0x38200000
[ 3.022900] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.028402] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus nu
mber 2
[ 3.036074] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 3.043448] hub 1-0:1.0: USB hub found
[ 3.047228] hub 1-0:1.0: 1 port detected
[ 3.051459] usb usb2: We don't know the algorithms for LPM for this host, dis
abling LPM.
[ 3.059985] hub 2-0:1.0: USB hub found
[ 3.063762] hub 2-0:1.0: 1 port detected
[ 3.069008] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 7 mkt segment 2 su
pported-hw 0x80 0x4
[ 3.078702] Hot alarm is canceled. GPU3D clock will return to 64/64
[ 3.088334] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 3.112399] isi-m2m 32e00000.isi:m2m_device: Register m2m success for ISI.0
[ 3.119589] cfg80211: Loading compiled-in X.509 certificates for regulatory d
atabase
[ 3.124991] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 3.128551] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.141100] platform regulatory.0: Direct firmware load for regulatory.db fai
led with error -2
[ 3.149726] platform regulatory.0: Falling back to sysfs fallback for: regula
tory.db
[ 3.160762] ALSA device list:
[ 3.163736] No soundcards found.
[ 3.169017] EXT4-fs (mmcblk2p2): mounting ext3 file system using the ext4 sub
system
[ 3.217473] EXT4-fs (mmcblk2p2): 5 orphan inodes deleted
[ 3.222876] EXT4-fs (mmcblk2p2): recovery complete
[ 3.233360] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Q
uota mode: none.
[ 3.241955] VFS: Mounted root (ext3 filesystem) on device 179:2.
[ 3.248052] devtmpfs: mounted
[ 3.252149] Freeing unused kernel memory: 3328K
[ 3.256818] Run /sbin/init as init process
[ 3.345777] systemd[1]: System time before build time, advancing clock.
[ 3.374628] systemd[1]: systemd 253.1^ running in system mode (+PAM -AUDIT -S
ELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL
-ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUAL
ITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMO
N +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 3.406404] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 6.1-mickledore (mickledore)!

[ 3.474564] systemd[1]: Hostname set to <imx8mp-lpddr4-evk>.
[ 3.548272] systemd-sysv-generator[189]: SysV service '/etc/init.d/umountfs'
lacks a native systemd unit file. Automatically generating a unit file for compa
tibility. Please update package to include a native systemd unit file, in order
to make it more safe and robust.
[ 3.576499] systemd-sysv-generator[189]: SysV service '/etc/init.d/save-rtc.s
h' lacks a native systemd unit file. Automatically generating a unit file for co
mpatibility. Please update package to include a native systemd unit file, in ord
er to make it more safe and robust.
[ 3.600861] systemd-sysv-generator[189]: SysV service '/etc/init.d/sshd' lack
s a native systemd unit file. Automatically generating a unit file for compatibi
lity. Please update package to include a native systemd unit file, in order to m
ake it more safe and robust.
[ 3.624519] systemd-sysv-generator[189]: SysV service '/etc/init.d/single' la
cks a native systemd unit file. Automatically generating a unit file for compati
bility. Please update package to include a native systemd unit file, in order to
make it more safe and robust.
[ 3.649952] systemd-sysv-generator[189]: SysV service '/etc/init.d/rc.local'
lacks a native systemd unit file. Automatically generating a unit file for compa
tibility. Please update package to include a native systemd unit file, in order
to make it more safe and robust.
[ 3.675040] systemd-sysv-generator[189]: SysV service '/etc/init.d/reboot' la
cks a native systemd unit file. Automatically generating a unit file for compati
bility. Please update package to include a native systemd unit file, in order to
make it more safe and robust.
[ 3.700095] systemd-sysv-generator[189]: SysV service '/etc/init.d/sendsigs'
lacks a native systemd unit file. Automatically generating a unit file for compa
tibility. Please update package to include a native systemd unit file, in order
to make it more safe and robust.
[ 3.725569] systemd-sysv-generator[189]: SysV service '/etc/init.d/halt' lack
s a native systemd unit file. Automatically generating a unit file for compatibi
lity. Please update package to include a native systemd unit file, in order to m
ake it more safe and robust.
[ 3.755545] systemd-sysv-generator[189]: SysV service '/etc/init.d/umountnfs.
sh' lacks a native systemd unit file. Automatically generating a unit file for c
ompatibility. Please update package to include a native systemd unit file, in or
der to make it more safe and robust.
[ 4.020247] systemd[1]: Queued start job for default target Multi-User System
.
[ 4.072477] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 4.095153] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 4.119519] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 4.146811] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.169500] systemd[1]: Started Dispatch Password Requests to Console Directo
ry Watch.
[ OK ] Started Dispatch Password ?쫡s to Console Directory Watch.
[ 4.193441] systemd[1]: Started Forward Password Requests to Wall Directory W
atch.
[ OK ] Started Forward Password R?쫢ests to Wall Directory Watch.
[ 4.217442] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 4.237247] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 4.257218] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 4.273375] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 4.323692] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 4.349354] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 4.369827] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 4.389534] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.414395] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 4.437891] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.462020] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.482227] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.506227] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.530193] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.554270] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 4.593542] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 4.617045] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.657499] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.677560] systemd[1]: Kernel Trace File System was skipped because of an un
met condition check (ConditionPathExists=/sys/kernel/tracing).
[ 4.694706] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 4.717878] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 4.745567] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 4.781773] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 4.804985] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 4.818762] fuse: init (API version 7.37)
[ 4.829015] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 4.845522] systemd[1]: File System Check on Root Device was skipped because
of an unmet condition check (ConditionPathIsReadWrite=!/).
[ 4.874110] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.894350] systemd[1]: Load Kernel Modules was skipped because no trigger co
ndition checks were met.
[ 4.907260] systemd[1]: Starting Generate network units from Kernel command l
ine...
Starting Generate network ?쫡s from Kernel command line...
[ 4.931064] systemd-journald[204]: Collecting audit messages is enabled.
[ 4.932490] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.950425] EXT4-fs (mmcblk2p2): re-mounted. Quota mode: none.
[ 4.960547] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 4.981017] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 5.008193] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 5.029668] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Reached target Preparation for Network.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 5.367671] systemd-journald[204]: Received client request to flush runtime j
ournal.
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
[ 5.535664] audit: type=1334 audit(1677836960.184:2): prog-id=5 op=LOAD
[ 5.542365] audit: type=1334 audit(1677836960.192:3): prog-id=6 op=LOAD
Starting Rule-based Manage?쫋or Device Events and Files...
[ OK ] Mounted /var/volatile.
Starting Load/Save OS Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Configuration...
Starting Network Name Resolution...
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Network Configuration.
[ 6.149194] Generic PHY 30be0000.ethernet-1:01: attached PHY driver (mii_bus:
phy_addr=30be0000.ethernet-1:01, irq=POLL)
[ 6.163359] fec 30be0000.ethernet eth0: Link is Up - 100Mbps/Full - flow cont
rol rx/tx
[ 6.190946] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ
-0
[ 6.198730] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ
-1
[ OK ] Started 6.209682] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TY
PE_PAGE_POOL RxQ-2
;39mNetwork Time Synchronization.
[ 6.221900] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ
-3
[ 6.231432] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ
-4
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ 6.412355] remoteproc remoteproc0: imx-dsp-rproc is available
[ 6.417125] imx-dwmac 30bf0000.ethernet eth1: PHY [stmmac-1:01] driver [RTL82
11F Gigabit Ethernet] (irq=POLL)
[ 6.441159] imx-dwmac 30bf0000.ethernet eth1: No Safety Features support foun
d
[ 6.448501] imx-dwmac 30bf0000.ethernet eth1: IEEE 1588-2008 Advanced Timesta
mp supported
Starting sshd.socket...
[ 6.462040] imx-dwmac 30bf0000.ethernet eth1: registered PTP clock
[ 6.475319] imx-dwmac 30bf0000.ethernet eth1: FPE workqueue start
[ 6.481602] imx-dwmac 30bf0000.ethernet eth1: configuring for phy/rgmii-id li
nk mode
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ 6.509471] 8021q: adding VLAN 0 to HW filter on device eth1
[ 6.516021] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 6.533300] CAN device driver interface
[ OK ] Listening on sshd.socket.
[ 6.558119] imx-sdma 30bd0000.dma-controller: sdma or sdma firmware not ready
!
[ 6.567722] imx-uart 30860000.serial: We cannot prepare for the RX slave dma!
[ 6.584887] wm8962 2-001a: Failed to read ID register
[ 6.598079] caam 30900000.crypto: device ID = 0x0a16040100000100 (Era 9)
[ 6.604908] caam 30900000.crypto: job rings = 1, qi = 0
[ OK ] Created slice Slice /system/systemd[ 6.613253] caam-snvs 30370000.ca
am-snvs: ipid matched - 0x3e
-backlight.
[ 6.626635] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secu
re state
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ 6.671397] debugfs: File 'Playback' in directory 'dapm' already present!
[ 6.678258] debugfs: File 'Capture' in directory 'dapm' already present!
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Kernel Logging Service.
[ 6.740148] imx8_media_dev: module is from the staging directory, the quality
is unknown, you have been warned.
[ OK ] Started System Logging Service.
[ 6.756610] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 6.763205] unregister ISI channel: mxc_isi.0
Starting D-Bus System Message Bus...
[ OK ] Started Linux Firmware Loader Daemon.
[ 6.801360] imx-sdma 30e10000.dma-controller: firmware found.
[ 6.801461] imx-sdma 30bd0000.dma-controller: firmware found.
[ 6.813042] imx-sdma 30bd0000.dma-controller: loaded firmware 4.6
Starting Telephony service...
Starting /etc/rc.local Compatibility...
Starting LSB: Run /etc/rc.local if it exist...
ftp folder exist
Starting Load/Save Screen ?쫛f backlight:lvds_backlight...
[ 6.878153] audit: type=1334 audit(1677837087.100:4): prog-id=7 op=LOAD
[ 6.888160] audit: type=1334 audit(1677837087.108:5): prog-id=8 op=LOAD
Starting User Login Management...
Starting Permit User Sessions...
[ 6.922623] mlan: loading out-of-tree module taints kernel.
Starting Target Communication Framework agent...
[ OK ] Started TEE Supplicant.
[ OK ] Started Vsftpd ftp daemon.
Starting OpenSSH Key Generation...
[ OK ] Finished 6.994722] wlan: Loading MWLAN driver
1;39mLoad/Save Screen ?쫟 of backlight:lvds_backlight.
[ OK ] Finished Permit User Sessions.
[ 7.009790] wlan: Register to Bus Driver...
[ OK ] Reached target Hardware activated USB gadget.
[ OK ] Finished OpenSSH Key Generation.
[ 7.029311] wlan: Register to Bus Driver Done
[ 7.033730] wlan: Driver loaded successfully
[ 7.058433] input: audio-hdmi HDMI Jack as /devices/platform/sound-hdmi/sound
/card1/input1
[ OK ] Started User Login Management.
Starting Bluetooth service...
Starting Save/Restore Sound Card State...
[ OK ] Finished Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
[ 8.344369] caam algorithms registered in /proc/crypto
[ 8.352796] caam 30900000.crypto: caam pkc algorithms registered in /proc/cry
pto
[ 8.361181] caam 30900000.crypto: rng crypto API alg registered prng-caam
[ 8.368072] caam 30900000.crypto: registering rng-caam
[ 8.376087] Device caam-keygen registered
[ 8.389097] random: crng init done
[ OK ] Finished Load/Save OS Random Seed.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Telephony service.
[ OK ] Started Bluetooth service.
[ OK ] Reached target Bluetooth Support.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Target Communication Framework agent.
[ 8.514606] audit: type=1334 audit(1677837088.736:6): prog-id=9 op=LOAD
[ 8.522674] audit: type=1334 audit(1677837088.744:7): prog-id=10 op=LOAD
Starting Hostname Service...
[ OK ] Started Hostname Service.
[ 9.633084] Bluetooth: hci0: Opcode 0x c03 failed: -110
ifconfig: SIOCGIFFLAGS: No such device
[ OK ] Started LSB: Run /etc/rc.local if it exist.
[FAILED] Failed to start /etc/rc.local Compatibility.
See 'systemctl status rc-local.service' for details.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttymxc1.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
Starting Record Runlevel Change in UTMP...
[ OK ] Finished Record Runlevel Change in UTMP.

NXP i.MX Release Distro 6.1-mickledore imx8mp-lpddr4-evk ttymxc1

imx8mp-lpddr4-evk login: [ 11.649384] Bluetooth: hci0: Setting baudrate failed
(-110)
[ 13.665994] Bluetooth: hci0: Setting wake-up method failed (-110)

imx8mp-lpddr4-evk login: [ 18.402701] platform sound-wm8962: deferred probe pe
nding

imx8mp-lpddr4-evk login: root
[ 21.699112] audit: type=1334 audit(1677837101.920:8): prog-id=11 op=LOAD
[ 21.705905] audit: type=1334 audit(1677837101.928:9): prog-id=12 op=LOAD
[ 22.022404] audit: type=1006 audit(1677837102.244:10): pid=418 uid=0 old-auid
=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ 22.034855] audit: type=1300 audit(1677837102.244:10): arch=c00000b7 syscall=
64 success=yes exit=1 a0=8 a1=ffffd6074d00 a2=1 a3=1 items=0 ppid=1 pid=418 auid
=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm
="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ 22.060928] audit: type=1327 audit(1677837102.244:10): proctitle="(systemd)"
[ 22.068424] audit: type=1334 audit(1677837102.268:11): prog-id=13 op=LOAD
[ 22.075732] audit: type=1300 audit(1677837102.268:11): arch=c00000b7 syscall=
280 success=yes exit=8 a0=5 a1=ffffecf9b3f8 a2=90 a3=0 items=0 ppid=1 pid=418 au
id=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 co
mm="systemd" exe="/lib/systemd/systemd" key=(null)
[ 22.101166] audit: type=1327 audit(1677837102.268:11): proctitle="(systemd)"
[ 22.108271] audit: type=1334 audit(1677837102.280:12): prog-id=13 op=UNLOAD
[ 22.115279] audit: type=1334 audit(1677837102.280:13): prog-id=14 op=LOAD
root@imx8mp-lpddr4-evk:~#

0 件の賞賛
返信

2,311件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think your wifi module is connected to the M.2 connector.

m.2.png

 

Please check the signals and the GPIO pins (IOMUX setting in dts file) are setting up properly.

 

 

0 件の賞賛
返信