Hi all,
i want to use usb in device mode for that i did like below in dts file.
reg_usb_otg_vbus: regulator@0 {
compatible = "regulator-fixed";
reg = <0>;
regulator-name = "usb_otg_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio3 22 0>;
output-high;
enable-active-high;
};
reg_usb_h1_vbus: regulator@1 {
compatible = "regulator-fixed";
reg = <1>;
regulator-name = "usb_h1_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio1 29 0>;
enable-active-high;
};
pinctrl_usbotg: usbotggrp {
fsl,pins = <
MX6QDL_PAD_GPIO_1__USB_OTG_ID 0x17059
>;
};
&usbh1 {
vbus-supply = <®_usb_h1_vbus>;
status = "okay";
};
&usbotg {
vbus-supply = <®_usb_otg_vbus>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbotg>;
dr-mode="host";
output-high;
disable-over-current;
status = "okay";
};
My log when i am installing modules.
| root@imx6_fs_wcam:/home# insmod configfs.ko |
root@imx6_fs_wcam:/home# insmod libcomposite.ko
root@imx6_fs_wcam:/home# insmod usb_f_mass_storage.ko
movable=1_fs_wcam:/home# insmod g_mass_storage.ko file=/dev/mmcblk2p1 stall=0 re
Number of LUNs=8
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
Number of LUNs=1
LUN: removable file: /dev/mmcblk2p1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: userspace failed to provide iSerialNumber
g_mass_storage gadget: g_mass_storage ready
root@imx6_fs_wcam:/home#
and in dmesg i observed like this
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
When i connected usb cable from board to PC. i got like this:
root@imx6_fs_wcam:/home# ci_hdrc ci_hdrc.0: remove, state 4
usb usb1: USB disconnect, device number 1
ci_hdrc ci_hdrc.0: USB bus 1 deregistered
ci_hdrc ci_hdrc.0: timeout waiting for 00000800 in 12
i need to get like this :
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
and it should mount in PC .
can any one please help me to sort it out.
Thanks & regards,
Lavanya
Solved! Go to Solution.
Hi Qinghua Zhu,
for my board i need to do only file=/dev/mmcblk2p1.
I found the problem.
In dts file i commented following things after that it is working fine. and usb is mounting in PC.
/*&usbh1 {
vbus-supply = <®_usb_h1_vbus>;
status = "okay";
};
*/
Thanks & regards,
Lavanya
I didn't test your method, below is my script,FYI:
insmod configfs.ko
insmod libcomposite.ko
insmod usb_f_mass_storage.ko
insmod gadgetfs.ko
insmod g_mass_storage.ko file=/dev/mmcblk1p1
Hi Qinghua Zhu San,
Has the issue got resolved?
Thanks,
Ramya
Hi Qinghua Zhu,
for my board i need to do only file=/dev/mmcblk2p1.
I found the problem.
In dts file i commented following things after that it is working fine. and usb is mounting in PC.
/*&usbh1 {
vbus-supply = <®_usb_h1_vbus>;
status = "okay";
};
*/
Thanks & regards,
Lavanya
which bsp are you using?