Hi all
my build environment
android 5.0
touch ic: ft5x06
imx6q.
i use boundary device ft5x06 driver (linux-imx6/ft5x06_ts.c at boundary-imx_3.14.28_1.0.0_ga · boundarydevices/linux-imx6 · GitHub)) , and i modify the dts just like
ft5x06@38 {
compatible = "ft5x06,ft5x06-touch";
reg = <0x38>;
interrupt-parent = <&gpio3>;
interrupts = <17 2>;
wakeup-gpios = <&gpio3 17 1>;
};
Then the touch can work , but still some issue (the x,y position didn't mach to screen)
Any body can help me !!
like the movie
解決済! 解決策の投稿を見る。
Hi Warren,
You have two choices to specify your screen resolution if the firmware doesn't report it properly:
- Give the resolution as a kernel boot argument:
ft5x06_ts.screenres=800,480
- Integrate our last patch to the driver which reads the resolution of fb0:
Regards,
Gary
hey i have used this driver ..probing is not successful and i2c read and write not happening,how you solved this issue . I'm using 4.4.3 Android.
Hi Warren,
You have two choices to specify your screen resolution if the firmware doesn't report it properly:
- Give the resolution as a kernel boot argument:
ft5x06_ts.screenres=800,480
- Integrate our last patch to the driver which reads the resolution of fb0:
Regards,
Gary
HI Gary
the resolution is correct (1024 *600).
It's the same situation.when i leave the screen and move to other position ,sometimes the circle didn't move with my finger.
like the movie.
Dropbox - 檔案 2016-3-15 上午1 33 43.mov
HI igor
the same problem with Tom ,The apk can't open!
BR
Warren
Hi Warren,
In that case it seems our driver is not meant for this version of the controller you are using. Have you tried using the mainline edt-ft5x06 driver instead?
kernel/git/torvalds/linux.git - Linux kernel source tree
Regards,
Gary
HI Bisson
The driver is correct for my controller. (Ft5606) it's for ft5x06_ts.c(boundary device source code)
i set Debug mode to read messages, I find Some strange errors.
when my finger touch the screen and leave the screen , the printHex message show below.
0000018260012affffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 1, points[0].x = 608, points[0].y = 298
0000004260012affffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 0, points[0].x = 608, points[0].y = 298
00000102fa0148ffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 1, points[0].x = 762, points[0].y = 328
00000182f90148ffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 1, points[0].x = 761, points[0].y = 328
00000182f90148ffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 1, points[0].x = 761, points[0].y = 328
00000182f90148ffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 1, points[0].x = 761, points[0].y = 328
00000042f90148ffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff....
ft5x06: buttons = 0, points[0].x = -2131943424, points[0].y = 2
button=1 , meant touch screen.
button=0 , meant leave screen.
the Status "buttons = 0, points[0].x = -2131943424, points[0].y = 2" will cause my touch circle didn't sync with my moving finger .
from 00/00/00/42/f9/01/48 ---> transfer to points[i].x / points[i].y is wrong !!!
Did you have any idea ???
BR
Warren
Hi, I come cross the same peoblem as you,my touch circle didn't sync with my moving finger .my touch circle didn't sync with my moving finger .How did you solve it at last? Thanks
HI peng
i used the other solution instead of Ft5606 .
Hi,
Thanks youn ! my problem had solved!
Hi ,I have the same problem, but when I install the apk on android 5.0 by igor. The apk can't open .
Like this video, please help me,Thank you!!
Hi warren
seems hardware works ok, then one can try native android app like:
http://appslollipop.com/Apps_Touch-sensitivity-calibration_Lollipop.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------