Freescale is responsible for cpu dai.
Codec vendor is responsible for codec dai.
Customer is responsible for machine driver, which should follow the alsa asoc framework.
No any direct call to the cpu dai to code dai.
And it is alsa development, please be aware of those.
Freescale is responsible for cpu dai.
Codec vendor is responsible for codec dai.
Customer is responsible for machine driver, which should follow the alsa asoc framework.
No any direct call to the cpu dai to code dai.
And it is alsa development, please be aware of those.
For specific wm8962 settings you can refer refer to Wolfson resources:
http://opensource.wolfsonmicro.com/content/linux-drivers-wolfson-devices
http://www.cirrus.com/en/products/wm8962-62b.html
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Victor,
Could you help to give these command such as :
tinymix SLIM RX1 MUX:AIF1_PB
tinymix SLIM_0_RX Channels:One
tinymix RX4 MIX1 INP1:RX1
tinymix RX4 Digital Volume:50
tinymix SPK DAC Switch:1
tinymix SLIMBUS_0_RX Audio Mixer MultiMedia1:1
tinyplay xxxx.wav -D 0 -d 0
Thanks!
BRs,
Jack