How to use the "MIPI_DSI_CLKCTRL.DPHY_SEL" register in i.MX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the "MIPI_DSI_CLKCTRL.DPHY_SEL" register in i.MX7

639 Views
toshiharu_shimi
Contributor II

Hello,

i.MX7Dual can select "1.5Gbps D-PHY" or "1Gbps D-PHY" with the D-PHY Select bit in the register "MIPI_DSI_CLKCTRL.DPHY_SEL".

In what case should "1Gbps D-PHY" be selected?

toshiharu_shimi_0-1720690358795.png

 

 

Labels (1)
0 Kudos
Reply
3 Replies

619 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @toshiharu_shimi 

The DPHY_SEL bit is used to change the PHY version. 

When it is 0, is selected the 2nd generation running up to 1.5Gbps.

When it is 1, is selected the 1st generation running up to 1.0Gbps.

 

Best regards,

Salas.

0 Kudos
Reply

606 Views
toshiharu_shimi
Contributor II

Hello @Manuel_Salas 

Thank you for your reply.

Does it mean that there are two D-PHY hardware blocks and I can choose one of them?

toshiharu_shimi_0-1720744359903.png

Normally, should I choose the 1.5Gbps D-PHY? Are there any cases where I should choose the 1.0Gbps D-PHY?
Currently, my product is using the 1.0Gbps D-PHY, but it occasionally malfunctions.
Since changing to the 1.5Gbps D-PHY prevents these malfunctions, should I use the 1.5Gbps D-PHY?

0 Kudos
Reply

592 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @toshiharu_shimi 

 

Yes, your diagram can represent that DPHY_SEL bit is doing.

 

About of 1.0Gbps phy, unfortunately we have not documented when 1.0Gbps is needed to use, but is prefereable to use the default DPHY (1.5Gbps).

 

Best regards,

--... ...--

Salas.

0 Kudos
Reply