How to use the FSL FlexCAN Driver of MQX CAN1, CAN2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the FSL FlexCAN Driver of MQX CAN1, CAN2

ソリューションへジャンプ
24,402件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has question below.

In M4 of i.MX6 SoloX using the FSL FlexCAN Driver of MQX CAN1, CAN2 I would like to do the CAN sent and received through the port, please tell me the register settings for use this port in the M4 side.

ラベル(1)
0 件の賞賛
返信
1 解決策
23,909件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MQX has APIs for operation with flexcan, please refer to attached

MQX_IO_User_Guide.pdf Chapter 8 FSL FlexCAN Driver.

Example can be found in MQX folder ..mqx/examples/can.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
23,910件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MQX has APIs for operation with flexcan, please refer to attached

MQX_IO_User_Guide.pdf Chapter 8 FSL FlexCAN Driver.

Example can be found in MQX folder ..mqx/examples/can.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信