How to use the FSL FlexCAN Driver of MQX CAN1, CAN2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use the FSL FlexCAN Driver of MQX CAN1, CAN2

跳至解决方案
1,791 次查看
takashitakahash
Contributor III

Hi community.

Our customer has question below.

In M4 of i.MX6 SoloX using the FSL FlexCAN Driver of MQX CAN1, CAN2 I would like to do the CAN sent and received through the port, please tell me the register settings for use this port in the M4 side.

标签 (1)
0 项奖励
回复
1 解答
1,300 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MQX has APIs for operation with flexcan, please refer to attached

MQX_IO_User_Guide.pdf Chapter 8 FSL FlexCAN Driver.

Example can be found in MQX folder ..mqx/examples/can.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,301 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MQX has APIs for operation with flexcan, please refer to attached

MQX_IO_User_Guide.pdf Chapter 8 FSL FlexCAN Driver.

Example can be found in MQX folder ..mqx/examples/can.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复