How to use the FSL FlexCAN Driver of MQX CAN1, CAN2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the FSL FlexCAN Driver of MQX CAN1, CAN2

Jump to solution
1,771 Views
takashitakahash
Contributor III

Hi community.

Our customer has question below.

In M4 of i.MX6 SoloX using the FSL FlexCAN Driver of MQX CAN1, CAN2 I would like to do the CAN sent and received through the port, please tell me the register settings for use this port in the M4 side.

Labels (1)
0 Kudos
Reply
1 Solution
1,280 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MQX has APIs for operation with flexcan, please refer to attached

MQX_IO_User_Guide.pdf Chapter 8 FSL FlexCAN Driver.

Example can be found in MQX folder ..mqx/examples/can.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,281 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MQX has APIs for operation with flexcan, please refer to attached

MQX_IO_User_Guide.pdf Chapter 8 FSL FlexCAN Driver.

Example can be found in MQX folder ..mqx/examples/can.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply