Hello,
I have created an image by using Yocto dora release with the command;
bitbake fsl-gui-image
I want to use openCV inside this image. For this purpose I have compiled openCV and the samples with the commands;
bitbake opencv
bitbake opencv-samples
But the problem is, fsl-gui-image is not updated after I compiled the openCV. Is there a process that I need to do for merging openCV inside fsl-gui-image or do I need to create a new custom image? How can I use openCV?
Thanks&Best Regards,
Fikret Alim
解決済! 解決策の投稿を見る。
You need to add the recipe to the image. This can be done in a number of different ways. The simplest may be to add to the end of your build/conf/local.conf file:
CORE_IMAGE_EXTRA_INSTALL += "\
opencv \
opencv-samples \
"
Note that this will add OpenCV to EVERY image you try to make. See this link for more information https://community.freescale.com/docs/DOC-95059.
You need to add the recipe to the image. This can be done in a number of different ways. The simplest may be to add to the end of your build/conf/local.conf file:
CORE_IMAGE_EXTRA_INSTALL += "\
opencv \
opencv-samples \
"
Note that this will add OpenCV to EVERY image you try to make. See this link for more information https://community.freescale.com/docs/DOC-95059.
Dear Josh,
Thank you very much for your support. It is now compiled and added to image, but the problem is, I still can not use opencv. Now, I found an opencv folder inside /usr/share, but it does not include neither executable nor source code. It only includes a samples folder which contain some images and videos. Also, I can not find any opencv libraries.
I don't know if you have expertise on opencv, but do you know what should I do to use it now? Thank you for your support.
Best Regards,
Fikret Alim
Hi Friket,
I made a tutorial for it: http://imxcv.blogspot.com.br/2014/02/building-opencv-24x-for-freescales-imx6.html
regards,
Andre
Hi Andre Silva,
I want to disable phyton support in opencv2.4.bb.
can you please guide me how to do that.
I tried
EXTRA_OECMAKE = -DBUILD_PYTHON_SUPPORT=OFF \
but not working
Hi Fikrel,
Have you figured out how to use openCV on Yocto?
I have done the same steps as you, but don't know how to use OpenCV yet
TIA
I do have a little bit of experience with OpenCV, but I have only ever built it on Ubuntu (using x86 and Beableboard). First things first, do you have all of the necessary plugins? You will need ffmpeg, gstreamer, and a couple others too. From my experience, OpenCV is not an executable, it is a set of libraries that can be linked to your code when compiling. I have never used OpenCV with Yocto so I do not know what is included when it is build. If you want sample code you may have to compile from source.
This link helped me out a lot when I was first setting it up: http://www.ozbotz.org/opencv-installation-2-3-1/