Hi,
I see this thread was never concluded. I too would like to be able to update images from a running OS (i.e. for field updates).
According to the manual:
1. Run ImageUpdate.exe
2. Select the new image(*.sb)
3. Click OK. The image is updated and the system reboots.
4. Ensure that this startup is from new image.
5. A message is displayed asking the user to continue updating.
6. Click NO.
7. Power OFF the device and power ON.
8. After this startup, a message is displayed asking the user to recover.
9. Click YES to continue. The image is recovered and the system reboots.
10. Ensure that this startup is from the old image
Running ImageUpdate.exe does not seem to do anything. Can anyone confirm if this application is complete or if it needs further work.
Mark