hello,
I am currently using the imx6ul-14X14-evk board, and I want to change the boot mode to "Boot From Fuses Mode".
I'm currently using NAND Flash boot. The Nandflash model is "MT29F32G08CBADBWP".
When I use SW602[1:2]= (ON, OFF) and SW601[1:4]= (ON, ON, OFF, ON), I can work normally.
Questions:
1. How can I modify eFuse to make the board work properly when using "Boot From Fuses Mode"?
I tried to set it up as follow ,but The chip doesn't seem to start,so how do I set it? Are these settings reversible?
fuse prog -y 0 0 00328033
fuse prog -y 0 5 000000A1
2. What is the difference between "fuse override" and "fuse prog" ?
Please help me,thank you!
解決済! 解決策の投稿を見る。
Hi
fuse programming is not reversible, difference between "fuse override"
and "fuse prog" is described in
Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog
For booting from fuses one can check Chapter 8
System Boot i.MX 6UltraLite Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
fuse programming is not reversible, difference between "fuse override"
and "fuse prog" is described in
Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog
For booting from fuses one can check Chapter 8
System Boot i.MX 6UltraLite Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I ran follow command ,and I can start it normal.Thank you for your reply.
# Burn 0x460[4] - BT_FUSE_SEL
fuse prog -y 0 6 0x00000010# Burn 0x450[0-7] - BT_FUSE_SEL
fuse prog -y 0 5 0x000000B3# Burn 0x450[8-15] - BT_FUSE_SEL
fuse prog -y 0 5 0x00000800