Hi all,
I want to use OTG as a USB host I/F with i.MX6SL and have some question about it.
1.
According to P9 of the EVK schematic, USB_TYPE_A connector (J10) is using as a Host mode.
Can I use EVK's driver without any customize when I use USB_OTG2 port as a Host mode ?
2
In my understanding, I need to set a ID pin to LOW when I use a OTG port as a Host mode.
However, EVK doesn't do anything.
Do I need any HW cutomeization when I use as a Host I/F ?
Ko-hey
已解决! 转到解答。
Hi Ko-hey
1. please try units tests (imx-test) (for example 045-Device-Host-Only-Test.txt):
.../test/mxc_usb_test/, read guidelines in /DOC folder
http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/
2. ID pin is absent in USB_TYPE_A connector, no need to set ID pin low
For description and usage ID pin please read usb2.0 specification on usb.org
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
1. please try units tests (imx-test) (for example 045-Device-Host-Only-Test.txt):
.../test/mxc_usb_test/, read guidelines in /DOC folder
http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/
2. ID pin is absent in USB_TYPE_A connector, no need to set ID pin low
For description and usage ID pin please read usb2.0 specification on usb.org
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
I believe you can find it in Demo image, probably using find
Tips For Linux - How to find files in Linux using 'find'
Best regards
igor