How to use SB_loader to load imx in parallel to multiple devices via USB.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use SB_loader to load imx in parallel to multiple devices via USB.

1,013 Views
idan357
Contributor I

Hello All.

Im trying to use SB_loader.xex when i have 4 mx6 devices connected to usb and i want to load them im parallel.

I there a way to direct the SB_loader to a specific USB ? form my tries i noticed the he only load the first usb he encounter.

I didnt see any flag that i can set to direct it to a specific USB port.

BR,

Idan.

0 Kudos
Reply
1 Reply

894 Views
igorpadykov
NXP Employee
NXP Employee

Hi Idan

I am afraid currently this is not supported, probably one can try to

modify application using sources

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply