How to use Pico Pi imx7d pin PWM2.OUT as a output ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Pico Pi imx7d pin PWM2.OUT as a output ?

514 Views
lucas_tanure
Contributor I

From PICO-PI_GL REVB1 schematics I can see pin 33 connected to PWM2.OUT, but where this pins is at the imx7 processor ? Which GPIO ? 

And how to configure it as output ?

Thanks

Lucas

0 Kudos
1 Reply

437 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lucas

pinout can be found in Table 92. i.MX 7Solo 12 x 12 mm functional contact assignments

i.MX7S Datasheet

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7SCEC.pdf

and sect.8.1 External Signals and Pin Multiplexing i.MX7S Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7SRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos