From PICO-PI_GL REVB1 schematics I can see pin 33 connected to PWM2.OUT, but where this pins is at the imx7 processor ? Which GPIO ?
And how to configure it as output ?
Thanks
Lucas
Hi Lucas
pinout can be found in Table 92. i.MX 7Solo 12 x 12 mm functional contact assignments
i.MX7S Datasheet
http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7SCEC.pdf
and sect.8.1 External Signals and Pin Multiplexing i.MX7S Reference Manual
http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7SRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------