Hi all,
I am trying to testing a PN532 module. This module support to connect to core board with I2C, SPI, HSU. I connect this module with UART3 on iMX8M Plus EVK board(EXP_CN PIN 8/10). But I cannot get any info with stty or minicom. BTW, I get nothing when i shot pin-8 and pin-10
I did not update image in the EMMC
Someone could have some advice?
Sry Sir,
I check the dts file of imx8mp-evk, and the uart is set as below
However, I cannot get anything with connecting the pin of UART3_TX and UART3_RX
Is there any other problems?
Thank u very much.
Hi, Rita Wang,
Could you please let me know if the PN7160 can be used with the libnfc-nci library? I read AN11697, which is a guide for using libnfc-nci with PN7120 and PN7150. However, I couldn't find any information indicating that this library supports the PN7160.
In addition, if the kernel driver nxp-pn5xx also supports PN7160 or not?
By the way, I'm going to integrate a NFC module into a linux board based on I.MX 8MPLUS, and we plan to use PN7160 for the advice from NXP official website
Hi @NealZhang ,
I already ask our NFC engineer Daniel help it in the new case 00645499, he will follow you and update to there, you can check in the email when he give update.
Wish you have a nice day
Best Regards
Rita