How to use PCIE internal PLL on imx8mplus platform .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use PCIE internal PLL on imx8mplus platform .

5,253 Views
t2865k5
Contributor I

Dear NXP ,

HW : srg_imx8mplus

SW : kernel version : 5.10.9

Because srg_imx8mplus PCIE is not connected to an oscillator, I modified the content of imx8mp-evk.dts as follows:

ext_osc = <0>;

I connected the PCIE device to the srg_imx8mplus platform ,and ran the lspci command. I did not see any message.

I check the imx8mp_pcie0.log . The message is as follows:

.....

 PLL REF_CLK is used!.

....

I don’t see the PCIE Link up message .

 

Could you tell me how to use PCIE internal PLL on imx8mplus platform ?

t2865k5_0-1640336146450.png

 

 

 

 

0 Kudos
Reply
8 Replies

5,191 Views
t2865k5
Contributor I

Hi igor ,

srg_imx8mplus platform:
It connects to another board with PCIE device through the connector.
I can't use general PCIE card on the srgimx8mplus platform.

This is the new PCIE board we designed.
I can't confirm that the PCIE board hardware is ok.

I modify device tree: osc = <0>;
When it boot , I measured
the PCIE_CLKN pin ,and it appear oscillating waveform . The oscillating waveform disappear within 2 seconds.
log:
imx6_pcie_host_init
imx6q-pcie 33800000.pcie: invalid resource
imx6q-pcie 33800000.pcie: Phy link never came up

ret = dw_pcie_wait_for_link(pci);


imx6q-pcie 33800000.pcie: ret=0xffffff92
imx6q-pcie 33800000.pcie: failed to initialize host

I have a question: When software set the internal PLL to output PCIE clock, the PCIE device is not connected.
It link fail ,and it will disable PLL clock.
Is my idea right?

0 Kudos
Reply

3,406 Views
emptyfridge
Contributor III

Hi all,

I have exactly the same behavior with imx8mm, try to use internal clk for PCIe. kernel 5.10.

       [    1.652640] imx6q-pcie 33800000.pcie: supply epdev_on not found, using dummy regulator
       [    1.667816] imx6q-pcie 33800000.pcie: PLL REF_CLK is used!.
       [    1.674263] imx6q-pcie 33800000.pcie: PCIe PLL locked after 20 us.
       [    1.683330] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
       [    1.690581] imx6q-pcie 33800000.pcie:       IO 0x001ff80000..0x001ff8ffff -> 0x0000000000
       [    1.707443] imx6q-pcie 33800000.pcie:      MEM 0x0018000000..0x001fefffff -> 0x0018000000
       [    1.715803] imx6q-pcie 33800000.pcie: invalid resource
       [    2.730995] imx6q-pcie 33800000.pcie: Phy link never came up
       [    2.736699] imx6q-pcie 33800000.pcie: failed to initialize host
       [    2.742628] imx6q-pcie 33800000.pcie: unable to add pcie port.

what I have in devtree:

    pcie0_refclk: pcie0-refclk {
        compatible = "fixed-clock";
        #clock-cells = <0>;
        clock-frequency = <100000000>;
    };


.............
        pinctrl_pcie0: pcie0grp {
            fsl,pins = <
                MX8MM_IOMUXC_I2C4_SCL_PCIE1_CLKREQ_B    0x61 
                MX8MM_IOMUXC_SPDIF_TX_GPIO5_IO3         0x41    /* AF9 WAKE */
                MX8MM_IOMUXC_SPDIF_EXT_CLK_GPIO5_IO5    0x41    /* AGF8 PERST  */
            >;
        };

............

&pcie0{
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_pcie0>;
    reset-gpio = <&gpio5 5 GPIO_ACTIVE_LOW>;
    clocks = <&clk IMX8MM_CLK_PCIE1_ROOT>,
        <&clk IMX8MM_CLK_PCIE1_AUX>,
        <&clk IMX8MM_CLK_PCIE1_PHY>,
        <&pcie0_refclk>;
    clock-names = "pcie", "pcie_aux", "pcie_phy", "pcie_bus";
    assigned-clocks = <&clk IMX8MM_CLK_PCIE1_AUX>,
                <&clk IMX8MM_CLK_PCIE1_PHY>,
                <&clk IMX8MM_CLK_PCIE1_CTRL>;
    assigned-clock-rates = <10000000>, <100000000>, <250000000>;
    assigned-clock-parents = <&clk IMX8MM_SYS_PLL2_50M>,
                <&clk IMX8MM_SYS_PLL2_100M>,
                <&clk IMX8MM_SYS_PLL2_250M>;
    ext_osc = <0>;
    status = "okay";
};

 

Same with the measuring. I can see the clock for about 2 seconds and then it stops.

Is there any new hints for that?

0 Kudos
Reply

5,188 Views
igorpadykov
NXP Employee
NXP Employee

yes right.

 

Best regards
igor

0 Kudos
Reply

5,213 Views
t2865k5
Contributor I

Hi Igor ,

(1) imx8mplus platform: imx8mp-evk.dts ext_osc = <0>;
It can measure the PCIE_CLKN waveform
(2) srg_imx8mplus platform: imx8mp-evk.dts ext_osc = <0>;
The PCIE_CLKN waveform can be measured when starting up, and the oscillating waveform will disappear after 5 seconds.
(3) I have a question, in pci-imx6.c:
imx6_pcie_init_phy() {
..
case IMX8MP:
case IMX8MP_EP:
}

IMX8MM: According to the value of imx6_pcie->ext_osc to set
External clock and internal PLL settings. But case IMX8MP : The imx6_pcie->ext_osc variable is not set ,so no matter the value of imx6_pcie->ext_osc is 0 or 1, it will be the output of the external clock. Is my idea correct?

0 Kudos
Reply

5,210 Views
igorpadykov
NXP Employee
NXP Employee

> But case IMX8MP : The imx6_pcie->ext_osc variable is not set ,so no matter the value of >imx6_pcie->ext_osc is 0 or 1, it will be the output of the external clock. Is my idea correct?

 

please look at (imx6_pcie->ext_osc is 0 or 1 is correctly handled):

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/pci/controller/dwc/pci-imx6.c?h=lf...

 

Best regards
igor

0 Kudos
Reply

5,232 Views
t2865k5
Contributor I

Dear Igorpadykov ,

I hope to simplify the problem. I measured the signal on the PCIE_CLKP pin, and there is no oscillation waveform.

How to solve this problem ?

0 Kudos
Reply

5,227 Views
igorpadykov
NXP Employee
NXP Employee

to narrow down issue if it is caused by hardware or software, please try to reproduce

issue on i.MX8M Plus EVK board.

 

Best regards
igor

 

 

0 Kudos
Reply

5,248 Views
igorpadykov
NXP Employee
NXP Employee

Hi Albert

 

in general for internal clock only ext_osc = <0>; change is needed.

May be recommended to check clock with oscilloscope and try with several pcie cards.

 

Best regards
igor

0 Kudos
Reply