Hi,
I am working over IMX6 based solo board . In my design , NOR Flash is interfaced with IMX6 solo. How to use MFG tool to flash the uboot and kernel over the NOR Flash. Does this tool work with JTAG interface ? or require any other interface. Please suggest.
Regards,
Aditya Nagal
Hello Aditya,
The MFG Tool, uses the USB Serial Downloader to load into the RAM of the system a micro Linux in order to flash your media, the commands of the Micro Linux to flash, it is just like a dd command, you can review the User Guide in the Documentation folder of the installation of the MFG Tool. The commands are call from an XML file.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------