How to use LVDS and HDMILVDS HDMI on MCIMX6QP-SDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use LVDS and HDMILVDS HDMI on MCIMX6QP-SDB

793 次查看
danny_li
Contributor II
Hi All
   evaluation board: MCIMX6QP-SDB      Linux BSP:4.14.78_1.0.0 ;
  image: fsl-image-qt5-validation-imx-imx6qsabresd-20200413075132.rootfs.bz2;
 1. I need to implement the display function,use HDMI or LVDS,use one of them,Which parameters need to be set, Are there application notes or guidance documents?
  2. What do I need to set in the boot and kernel, I'm confused right now,About the use of the new version of BSP,Debugging  HDMI display  or LVDS display, Can you provide some guidance documents, thanks.
 
标签 (1)
0 项奖励
回复
1 回复

646 次查看
radhikasomaiya
Senior Contributor II

Hi danny.li@weikeng.com.cn ,

For HDMI and LVDS display you can set mmcargs using u-boot setenv command.

      HDMI
            setenv displayinfo 'video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'
            setenv mmcargs ${mmcargs} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

      LVDS
            setenv displayinfo 'video=mxcfb0:dev=ldb,if=RGB666'
            setenv mmcargs ${mmcargs} video=mxcfb0:dev=ldb,if=RGB666

For different display you can refer Specifying display section from section 4.7 Running Linux OS on the target of i.MX Linux User's guide as per below.

Screenshot (43).png

Regards 

Radhika Somaiya.