How to use Flexray to iMX6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use Flexray to iMX6?

1,349 次查看
wangben
Contributor I

Hi ,

I used iMX6 in my project, I want to use Flexray and choice MFR4310+ TJA1080, but MFR4310 is using Asynchronous Memory Interface.

How to connect MFR4310 to iMX6? If it can not to do, which the solution of Flexray is good?

B.R

Ben

0 项奖励
回复
2 回复数

1,141 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Wang,

  The only way  that I see to interface it, it is using the  EIM interface, just like it shows the reference manual of the MFR4310 in the figure 2.7.  MPC Interface with MPC5xx and MPC5xxx Families.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,141 次查看
wangben
Contributor I

Hi James,

Thanks! I will study it.

Ben

0 项奖励
回复