Dear all,
Please let me know about how to use EIM of i.MX6 DL/Solo
The page 1036 in a reference manual ( http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf )
About the function of bit23 (AUS) in 22.9.1 Chip Select n General Configuration Register 1 (EIM_CSnGCR1)
a) in the case of DSZ = 001 : 16 bit port resides on DATA[15:0]
or 010 : 16 bit port resides on DATA[31:16]
b) in the case of DSZ = 011 : 32 bit port resides on DATA[31:0]
Is my understanding correct?
Best Regards,
George
Solved! Go to Solution.
Hi George
yes correct, also it may be useful to check
sect.4.9.3.1 "EIM Interface Pads Allocation" IMX6SDLCEC
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi George
yes correct, also it may be useful to check
sect.4.9.3.1 "EIM Interface Pads Allocation" IMX6SDLCEC
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear chip,
Please let me know one more.
The information on an AUS bit is not included in Section 4.9.3.1 - Table 37.
Is my following understanding correct?
BR,
George
Hi George
yes this understanding is correct.
Best regards
Dear igorpadykov,
Thanks.
BR,
George
Dear chip,
Thanks.
BR,
George