How to use DDR Stress Tester V1.0.3 for imx6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use DDR Stress Tester V1.0.3 for imx6?

2,448 Views
jiangshao
Contributor V

I want to use DDR_Stress_Tester_V1.0.3 for imx6 sabresd(imx6dl, 2GB RAM, chip is H5TQ4G63MFR-PBC x 4).

“DDR_Stress_Tester -t mx6x -df mx6x_ddr_script_filename”

Which script file should I use?

MX6DL_ARD_DDR3_register_programming_aid_v0.2.inc or

MX6DL_SabreSD_DDR3_register_programming_aid_v1.5.inc?

Labels (4)
0 Kudos
5 Replies

715 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiang

for sabresd one needs to use *SabreSD* file.

If you are testing own custom board - then script aid on link below

i.Mx6DQSDL DDR3 Script Aid

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

715 Views
jiangshao
Contributor V

Thank you for your reply.

I got the following result.

It means there are something wrong with memory?

And I think I need to update flash_header.S(uboot-imx) according to the output results,

but there is no explanation for this in User Guide.

How should I update flash_header.S based on the output?

-------------------------------------

P:\DDR_Stress_Tester_V1.0.3\Binary>DDR_Stress_Tester -t mx6x -df MX6DL_SabreSD_D

DR3_register_programming_aid_v1.5.inc

MX6DL opened.

HAB_TYPE: DEVELOP

Image loading...

download Image to IRAM OK

Re-open MX6x device.

Running DDR test..., press "ESC" key to exit.

******************************

    DDR Stress Test (1.0.3) for MX6DL

    Build: Jun 25 2014, 12:09:29

    Freescale Semiconductor, Inc.

******************************

=======DDR configuration==========

BOOT_CFG3[5-4]: 0x00, Single DDR channel.

DDR type is DDR3

Data width: 64, bank num: 8

Row size: 14, col size: 10

Chip select CSD0 is used

Density per chip select: 1024MB

==================================

What ARM core speed would you like to run?

Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz

  ARM set to 1GHz

Please select the DDR density per chip select (in bytes) on the board

Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6

for 32MB

For maximum supported density (4GB), we can only access up to 3.75GB.  Type 9 to

select this

  DDR density selected (MB): 2048

Calibration will run at DDR frequency 400MHz. Type 'y' to continue.

If you want to run at other DDR frequency. Type 'n'

  DDR Freq: 396 MHz

Would you like to run the write leveling calibration? (y/n)

  Please enter the MR1 value on the initilization script

  This will be re-programmed into MR1 after write leveling calibration

  Enter as a 4-digit HEX value, example 0004, then hit enter

0004 You have entered: 0x0004

Start write leveling calibration

Write leveling calibration completed

MMDC_MPWLDECTRL0 ch0 after write level cal: 0x003B003F

MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00320033

MMDC_MPWLDECTRL0 ch1 after write level cal: 0x0011001C

MMDC_MPWLDECTRL1 ch1 after write level cal: 0x00140022

Would you like to run the DQS gating, read/write delay calibration? (y/n)

Starting DQS gating calibration...

. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .

. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .

BYTE 0:

        Start:           HC=0x00 ABS=0x30

        End:             HC=0x03 ABS=0x6C

        Mean:            HC=0x02 ABS=0x0E

        End-0.5*tCK:     HC=0x02 ABS=0x6C

        Final:           HC=0x02 ABS=0x6C

BYTE 1:

        Start:           HC=0x01 ABS=0x2C

        End:             HC=0x03 ABS=0x6C

        Mean:            HC=0x02 ABS=0x4C

        End-0.5*tCK:     HC=0x02 ABS=0x6C

        Final:           HC=0x02 ABS=0x6C

BYTE 2:

        Start:           HC=0x00 ABS=0x2C

        End:             HC=0x03 ABS=0x5C

        Mean:            HC=0x02 ABS=0x04

        End-0.5*tCK:     HC=0x02 ABS=0x5C

        Final:           HC=0x02 ABS=0x5C

BYTE 3:

        Start:           HC=0x00 ABS=0x28

        End:             HC=0x03 ABS=0x5C

        Mean:            HC=0x02 ABS=0x02

        End-0.5*tCK:     HC=0x02 ABS=0x5C

        Final:           HC=0x02 ABS=0x5C

BYTE 4:

        Start:           HC=0x01 ABS=0x10

        End:             HC=0x03 ABS=0x58

        Mean:            HC=0x02 ABS=0x34

        End-0.5*tCK:     HC=0x02 ABS=0x58

        Final:           HC=0x02 ABS=0x58

BYTE 5:

        Start:           HC=0x01 ABS=0x0C

        End:             HC=0x03 ABS=0x54

        Mean:            HC=0x02 ABS=0x30

        End-0.5*tCK:     HC=0x02 ABS=0x54

        Final:           HC=0x02 ABS=0x54

BYTE 6:

        Start:           HC=0x01 ABS=0x04

        End:             HC=0x03 ABS=0x4C

        Mean:            HC=0x02 ABS=0x28

        End-0.5*tCK:     HC=0x02 ABS=0x4C

        Final:           HC=0x02 ABS=0x4C

BYTE 7:

        Start:           HC=0x01 ABS=0x00

        End:             HC=0x03 ABS=0x40

        Mean:            HC=0x02 ABS=0x20

        End-0.5*tCK:     HC=0x02 ABS=0x40

        Final:           HC=0x02 ABS=0x40

DQS calibration MMDC0 MPDGCTRL0 = 0x426C026C, MPDGCTRL1 = 0x025C025C

DQS calibration MMDC1 MPDGCTRL0 = 0x42540258, MPDGCTRL1 = 0x0240024C

Note: Array result[] holds the DRAM test result of each byte.

      0: test pass.  1: test fail

      4 bits respresent the result of 1 byte.

      result 00000001:byte 0 fail.

      result 00000011:byte 0, 1 fail.

Starting Read calibration...

ABS_OFFSET=0x00000000   result[00]=0x11111111

ABS_OFFSET=0x04040404   result[01]=0x11111111

ABS_OFFSET=0x08080808   result[02]=0x11111111

ABS_OFFSET=0x0C0C0C0C   result[03]=0x11111111

ABS_OFFSET=0x10101010   result[04]=0x11111111

ABS_OFFSET=0x14141414   result[05]=0x11111111

ABS_OFFSET=0x18181818   result[06]=0x11111011

ABS_OFFSET=0x1C1C1C1C   result[07]=0x01100011

ABS_OFFSET=0x20202020   result[08]=0x00100010

ABS_OFFSET=0x24242424   result[09]=0x00000000

ABS_OFFSET=0x28282828   result[0A]=0x00000000

ABS_OFFSET=0x2C2C2C2C   result[0B]=0x00000000

ABS_OFFSET=0x30303030   result[0C]=0x00000000

ABS_OFFSET=0x34343434   result[0D]=0x00000000

ABS_OFFSET=0x38383838   result[0E]=0x00000000

ABS_OFFSET=0x3C3C3C3C   result[0F]=0x00000000

ABS_OFFSET=0x40404040   result[10]=0x00000000

ABS_OFFSET=0x44444444   result[11]=0x00000000

ABS_OFFSET=0x48484848   result[12]=0x00000000

ABS_OFFSET=0x4C4C4C4C   result[13]=0x00000000

ABS_OFFSET=0x50505050   result[14]=0x00000000

ABS_OFFSET=0x54545454   result[15]=0x00000000

ABS_OFFSET=0x58585858   result[16]=0x00000000

ABS_OFFSET=0x5C5C5C5C   result[17]=0x00000000

ABS_OFFSET=0x60606060   result[18]=0x00000000

ABS_OFFSET=0x64646464   result[19]=0x00000000

ABS_OFFSET=0x68686868   result[1A]=0x00000000

ABS_OFFSET=0x6C6C6C6C   result[1B]=0x10000000

ABS_OFFSET=0x70707070   result[1C]=0x11001100

ABS_OFFSET=0x74747474   result[1D]=0x11001100

ABS_OFFSET=0x78787878   result[1E]=0x11111111

ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

MMDC0 MPRDDLCTL = 0x44424C4A, MMDC1 MPRDDLCTL = 0x42464C48

Starting Write calibration...

ABS_OFFSET=0x00000000   result[00]=0x10101100

ABS_OFFSET=0x04040404   result[01]=0x10001000

ABS_OFFSET=0x08080808   result[02]=0x10001000

ABS_OFFSET=0x0C0C0C0C   result[03]=0x00000000

ABS_OFFSET=0x10101010   result[04]=0x00000000

ABS_OFFSET=0x14141414   result[05]=0x00000000

ABS_OFFSET=0x18181818   result[06]=0x00000000

ABS_OFFSET=0x1C1C1C1C   result[07]=0x00000000

ABS_OFFSET=0x20202020   result[08]=0x00000000

ABS_OFFSET=0x24242424   result[09]=0x00000000

ABS_OFFSET=0x28282828   result[0A]=0x00000000

ABS_OFFSET=0x2C2C2C2C   result[0B]=0x00000000

ABS_OFFSET=0x30303030   result[0C]=0x00000000

ABS_OFFSET=0x34343434   result[0D]=0x00000000

ABS_OFFSET=0x38383838   result[0E]=0x00000000

ABS_OFFSET=0x3C3C3C3C   result[0F]=0x00000000

ABS_OFFSET=0x40404040   result[10]=0x00000000

ABS_OFFSET=0x44444444   result[11]=0x00000000

ABS_OFFSET=0x48484848   result[12]=0x00000000

ABS_OFFSET=0x4C4C4C4C   result[13]=0x00000000

ABS_OFFSET=0x50505050   result[14]=0x00000010

ABS_OFFSET=0x54545454   result[15]=0x00000010

ABS_OFFSET=0x58585858   result[16]=0x00010010

ABS_OFFSET=0x5C5C5C5C   result[17]=0x00010010

ABS_OFFSET=0x60606060   result[18]=0x01110011

ABS_OFFSET=0x64646464   result[19]=0x11110011

ABS_OFFSET=0x68686868   result[1A]=0x11111111

ABS_OFFSET=0x6C6C6C6C   result[1B]=0x11111111

ABS_OFFSET=0x70707070   result[1C]=0x11111111

ABS_OFFSET=0x74747474   result[1D]=0x11111111

ABS_OFFSET=0x78787878   result[1E]=0x11111111

ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

MMDC0 MPWRDLCTL = 0x3834262E,MMDC1 MPWRDLCTL = 0x362E302A

   MMDC registers updated from calibration

   Read DQS Gating calibration

   MPDGCTRL0 PHY0 (0x021b083c) = 0x426C026C

   MPDGCTRL1 PHY0 (0x021b0840) = 0x025C025C

   MPDGCTRL0 PHY1 (0x021b483c) = 0x42540258

   MPDGCTRL1 PHY1 (0x021b4840) = 0x0240024C

   Read calibration

   MPRDDLCTL PHY0 (0x021b0848) = 0x44424C4A

   MPRDDLCTL PHY1 (0x021b4848) = 0x42464C48

   Write calibration

   MPWRDLCTL PHY0 (0x021b0850) = 0x3834262E

   MPWRDLCTL PHY1 (0x021b4850) = 0x362E302A

The DDR stress test can run with an incrementing frequency or at a static freq

To run at a static freq, simply set the start freq and end freq to the same valu

e

Would you like to run the DDR Stress Test (y/n)?

Enter desired START freq (135 to 672 MHz), then hit enter.

Note: DDR3 minimum is ~333MHz, do not recommend to go too much below this.

528

  The freq you entered was: 528

Enter desired END freq (135 to 672 MHz), then hit enter.

Make sure this is equal to or greater than start freq

550

  The freq you entered was: 550

Beginning stress test

loop: 1

DDR Freq: 528 MHz

t0.1: data is addr test

Address of failure: 0x50000000

Data was: 0x4fff00c0

But pattern  should match address

0 Kudos

715 Views
igorpadykov
NXP Employee
NXP Employee

if you are using custom board, you should not

use  DDR3_register_programming_aid_v1.5.inc.

Instead one needs to create custom *.inc file

for your memory  - "chip is H5TQ4G63MFR-PBC x 4",

based on results https://community.freescale.com/docs/DOC-94917

0 Kudos

715 Views
JithCR
Contributor III

Hi Igor,

I am using DDR_Stress_Tester_V1.0.3_20_08_2014 for checking DDR3 for one of the non-booting i.MX6Q based custom board.

And I am getting below mentioned output for DDR stress test.

loop: 1

DDR Freq: 528 MHz

t0.1: data is addr test

Address of failure: 0x10000000

Data was: 0x00000000

But pattern  should match address

Its seems there is an issue in RAM.

But I am not able conclude that whether the issue in data line or in address lines.

I would like to know whether its possible to identify data lines/address line issue using DDR Stress Tester?

0 Kudos

715 Views
jiangshao
Contributor V

Thank u very much!

I refered to the data sheet of memory chip and https://community.freescale.com/docs/DOC-94917,

got the result as follow.

And I think I need to update flash_header.S(uboot-imx) according to the output results,

but there is no explanation for this in User Guide.

How should I update flash_header.S based on the output?

-----------

Would you like to run the write leveling calibration? (y/n)
  Please enter the MR1 value on the initilization script
  This will be re-programmed into MR1 after write leveling calibration
  Enter as a 4-digit HEX value, example 0004, then hit enter
0004 You have entered: 0x0004
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x00360039
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x002D0034
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x000E0017
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x00110023

Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .
. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .
BYTE 0:
        Start:           HC=0x01 ABS=0x34
        End:             HC=0x03 ABS=0x70
        Mean:            HC=0x02 ABS=0x52
        End-0.5*tCK:     HC=0x02 ABS=0x70
        Final:           HC=0x02 ABS=0x70
BYTE 1:
        Start:           HC=0x01 ABS=0x3C
        End:             HC=0x03 ABS=0x74
        Mean:            HC=0x02 ABS=0x58
        End-0.5*tCK:     HC=0x02 ABS=0x74
        Final:           HC=0x02 ABS=0x74
BYTE 2:
        Start:           HC=0x00 ABS=0x28
        End:             HC=0x03 ABS=0x64
        Mean:            HC=0x02 ABS=0x06
        End-0.5*tCK:     HC=0x02 ABS=0x64
        Final:           HC=0x02 ABS=0x64
BYTE 3:
        Start:           HC=0x01 ABS=0x28
        End:             HC=0x03 ABS=0x64
        Mean:            HC=0x02 ABS=0x46
        End-0.5*tCK:     HC=0x02 ABS=0x64
        Final:           HC=0x02 ABS=0x64
BYTE 4:
        Start:           HC=0x00 ABS=0x1C
        End:             HC=0x03 ABS=0x5C
        Mean:            HC=0x01 ABS=0x7B
        End-0.5*tCK:     HC=0x02 ABS=0x5C
        Final:           HC=0x02 ABS=0x5C
BYTE 5:
        Start:           HC=0x01 ABS=0x10
        End:             HC=0x03 ABS=0x58
        Mean:            HC=0x02 ABS=0x34
        End-0.5*tCK:     HC=0x02 ABS=0x58
        Final:           HC=0x02 ABS=0x58
BYTE 6:
        Start:           HC=0x01 ABS=0x14
        End:             HC=0x03 ABS=0x4C
        Mean:            HC=0x02 ABS=0x30
        End-0.5*tCK:     HC=0x02 ABS=0x4C
        Final:           HC=0x02 ABS=0x4C
BYTE 7:
        Start:           HC=0x01 ABS=0x08
        End:             HC=0x03 ABS=0x40
        Mean:            HC=0x02 ABS=0x24
        End-0.5*tCK:     HC=0x02 ABS=0x40
        Final:           HC=0x02 ABS=0x40

DQS calibration MMDC0 MPDGCTRL0 = 0x02740270, MPDGCTRL1 = 0x02640264

DQS calibration MMDC1 MPDGCTRL0 = 0x0258025C, MPDGCTRL1 = 0x0240024C

Note: Array result[] holds the DRAM test result of each byte.
      0: test pass.  1: test fail
      4 bits respresent the result of 1 byte.
      result 00000001:byte 0 fail.
      result 00000011:byte 0, 1 fail.

Starting Read calibration...

ABS_OFFSET=0x00000000   result[00]=0x11111111
ABS_OFFSET=0x04040404   result[01]=0x11111111
ABS_OFFSET=0x08080808   result[02]=0x11111111
ABS_OFFSET=0x0C0C0C0C   result[03]=0x11111111
ABS_OFFSET=0x10101010   result[04]=0x11111111
ABS_OFFSET=0x14141414   result[05]=0x11111111
ABS_OFFSET=0x18181818   result[06]=0x11111011
ABS_OFFSET=0x1C1C1C1C   result[07]=0x11111011
ABS_OFFSET=0x20202020   result[08]=0x01100011
ABS_OFFSET=0x24242424   result[09]=0x00000010
ABS_OFFSET=0x28282828   result[0A]=0x00000000
ABS_OFFSET=0x2C2C2C2C   result[0B]=0x00000000
ABS_OFFSET=0x30303030   result[0C]=0x00000000
ABS_OFFSET=0x34343434   result[0D]=0x00000000
ABS_OFFSET=0x38383838   result[0E]=0x00000000
ABS_OFFSET=0x3C3C3C3C   result[0F]=0x00000000
ABS_OFFSET=0x40404040   result[10]=0x00000000
ABS_OFFSET=0x44444444   result[11]=0x00000000
ABS_OFFSET=0x48484848   result[12]=0x00000000
ABS_OFFSET=0x4C4C4C4C   result[13]=0x00000000
ABS_OFFSET=0x50505050   result[14]=0x00000000
ABS_OFFSET=0x54545454   result[15]=0x00000000
ABS_OFFSET=0x58585858   result[16]=0x00000000
ABS_OFFSET=0x5C5C5C5C   result[17]=0x00000000
ABS_OFFSET=0x60606060   result[18]=0x00000000
ABS_OFFSET=0x64646464   result[19]=0x00000000
ABS_OFFSET=0x68686868   result[1A]=0x00000000
ABS_OFFSET=0x6C6C6C6C   result[1B]=0x00000000
ABS_OFFSET=0x70707070   result[1C]=0x00001000
ABS_OFFSET=0x74747474   result[1D]=0x10111111
ABS_OFFSET=0x78787878   result[1E]=0x11111111
ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

MMDC0 MPRDDLCTL = 0x46444C4A, MMDC1 MPRDDLCTL = 0x484C4A48

Starting Write calibration...

ABS_OFFSET=0x00000000   result[00]=0x11101111
ABS_OFFSET=0x04040404   result[01]=0x11101001
ABS_OFFSET=0x08080808   result[02]=0x00001000
ABS_OFFSET=0x0C0C0C0C   result[03]=0x00000000
ABS_OFFSET=0x10101010   result[04]=0x00000000
ABS_OFFSET=0x14141414   result[05]=0x00000000
ABS_OFFSET=0x18181818   result[06]=0x00000000
ABS_OFFSET=0x1C1C1C1C   result[07]=0x00000000
ABS_OFFSET=0x20202020   result[08]=0x00000000
ABS_OFFSET=0x24242424   result[09]=0x00000000
ABS_OFFSET=0x28282828   result[0A]=0x00000000
ABS_OFFSET=0x2C2C2C2C   result[0B]=0x00000000
ABS_OFFSET=0x30303030   result[0C]=0x00000000
ABS_OFFSET=0x34343434   result[0D]=0x00000000
ABS_OFFSET=0x38383838   result[0E]=0x00000000
ABS_OFFSET=0x3C3C3C3C   result[0F]=0x00000000
ABS_OFFSET=0x40404040   result[10]=0x00000000
ABS_OFFSET=0x44444444   result[11]=0x00000000
ABS_OFFSET=0x48484848   result[12]=0x00000000
ABS_OFFSET=0x4C4C4C4C   result[13]=0x00000000
ABS_OFFSET=0x50505050   result[14]=0x00000000
ABS_OFFSET=0x54545454   result[15]=0x00010000
ABS_OFFSET=0x58585858   result[16]=0x00010010
ABS_OFFSET=0x5C5C5C5C   result[17]=0x00010010
ABS_OFFSET=0x60606060   result[18]=0x01010010
ABS_OFFSET=0x64646464   result[19]=0x01111110
ABS_OFFSET=0x68686868   result[1A]=0x11111110
ABS_OFFSET=0x6C6C6C6C   result[1B]=0x11111111
ABS_OFFSET=0x70707070   result[1C]=0x11111111
ABS_OFFSET=0x74747474   result[1D]=0x11111111
ABS_OFFSET=0x78787878   result[1E]=0x11111111
ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

MMDC0 MPWRDLCTL = 0x36322C38,MMDC1 MPWRDLCTL = 0x36323428


   MMDC registers updated from calibration

   Read DQS Gating calibration
   MPDGCTRL0 PHY0 (0x021b083c) = 0x02740270
   MPDGCTRL1 PHY0 (0x021b0840) = 0x02640264
   MPDGCTRL0 PHY1 (0x021b483c) = 0x0258025C
   MPDGCTRL1 PHY1 (0x021b4840) = 0x0240024C

   Read calibration
   MPRDDLCTL PHY0 (0x021b0848) = 0x46444C4A
   MPRDDLCTL PHY1 (0x021b4848) = 0x484C4A48

   Write calibration
   MPWRDLCTL PHY0 (0x021b0850) = 0x36322C38
   MPWRDLCTL PHY1 (0x021b4850) = 0x36323428

-----------

0 Kudos