Hello community,
I have 2 question about CCM_CLPCR[STBY_COUNT] bit.
1) I think, that CCM wait counter count as following value. is it correct?
CCM_CGPR[0] = 0: pmic_delay_scaler = 1,
STBY_COUNT
00 : CCM wait (1 * 1)+ 1 = 2 CKIL cycle.
01 : CCM wait (3 * 1)+ 1 = 4 CKIL cycle.
10 : CCM wait (7 * 1)+ 1 = 8 CKIL cycle.
11 : CCM wait (15 * 1)+ 1 = 16 CKIL cycle.
CCM_CGPR[0] = 1: pmic_delay_scaler = 8,
STBY_COUNT
00 : CCM wait (1 * 8)+ 1 = 9 CKIL cycle.
01 : CCM wait (3 * 8)+ 1 = 25 CKIL cycle.
10 : CCM wait (7 * 8)+ 1 = 57 CKIL cycle.
11 : CCM wait (15 * 8)+ 1 = 121 CKIL cycle.
2) Which signal will start this counter?
Rise-up("0" -> "1") edge of PMIC_STBY_REQ pin?
or Some trigger to exit STOP mode?
to set CCM_CLCR[STBY_COUNT] bit, we need a start timing of wait cycle.
End time seems that all PMIC power source will wake up to functional voltage, I think.
Best regards,
Ishii.
已解决! 转到解答。
Hi Ishii
>1) I think, that CCM wait counter count as following value. is it correct?
correct
>2) Which signal will start this counter?
> Rise-up("0" -> "1") edge of PMIC_STBY_REQ pin?
yes it is PMIC_STBY_REQ and described in sect.18.5.3.3.2 Exiting STOP mode i.MX6DQ
Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
>to set CCM_CLCR[STBY_COUNT] bit, we need a start timing of wait cycle.
>End time seems that all PMIC power source will wake up to functional voltage, I think.
right
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ishii
>1) I think, that CCM wait counter count as following value. is it correct?
correct
>2) Which signal will start this counter?
> Rise-up("0" -> "1") edge of PMIC_STBY_REQ pin?
yes it is PMIC_STBY_REQ and described in sect.18.5.3.3.2 Exiting STOP mode i.MX6DQ
Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
>to set CCM_CLCR[STBY_COUNT] bit, we need a start timing of wait cycle.
>End time seems that all PMIC power source will wake up to functional voltage, I think.
right
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------