How to use ARM DS-5 to compile the demo of FreeRTOS in window 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use ARM DS-5 to compile the demo of FreeRTOS in window 10

跳至解决方案
1,887 次查看
jingyangxie
Contributor V

Recently,I have bought a imx6sxsabresd board,I want to run applications on Cortex m4,When I followed the steps in <<Getting_Started_with_FreeRTOS_BSP_for_i.MX_6SoloX.pdf>>,It reported some errors when I compile the hello_world demo. as follows:

pastedImage_0.png

how does this happened ?

标签 (3)
0 项奖励
回复
1 解答
1,694 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  jingyang

one can check if necessary toolchain is installed, please refer to sect.

3 Development Tools attached Release notes and steps for toolchain installation in

Adding New Compiler Toolchains to DS-5 – DS-5 Development Studio – ARM Developer

or p.8 AN5229 ARM DS-5 Development Studio Debug

http://www.nxp.com/files/32bit/doc/app_note/AN5229.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,695 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  jingyang

one can check if necessary toolchain is installed, please refer to sect.

3 Development Tools attached Release notes and steps for toolchain installation in

Adding New Compiler Toolchains to DS-5 – DS-5 Development Studio – ARM Developer

or p.8 AN5229 ARM DS-5 Development Studio Debug

http://www.nxp.com/files/32bit/doc/app_note/AN5229.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------