How to update boot image and device tree to android 13 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update boot image and device tree to android 13 ?

1,799件の閲覧回数
t2865k5
Contributor I

Dear NXP ,

HW : imx8mplus
SDK :imx-android-13.0.0_2.2.0

 

 

source build/envsetup.sh

lunch evk_8mp-userdebug

 

./imx-make.sh bootloader kernel -j4 2>&1 | tee build-log.txt

make -j4 2>&1 | tee -a build-log.txt

 

Flash android image to 16GB sd card:

./imx-sdcard-partition.sh -f imx8mp -D ../imx8mp_android/imx-android-13.0.0_2.2.0/android_build/out/target/product/evk_8mp /dev/sdb

 

I Build a new boot image (Image , imx8mp-evk.dtb)

How can I update boot image and device tree to sd card ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,612件の閲覧回数
t2865k5
Contributor I

Dear NXP ,

We don't provide UUU hardware interface in my project . So, I can't use uuu tool in my project .

Could you tell me how to use linux command to update u-boot and kernel image .

Ex:

u-boot : sudo dd if=imx-boot-imx8mpevk-sd.bin-flash_evk of=/dev/sdb bs=1k seek=32 conv=sync

kernel : sudo cp Image /media/username/boot/

 

0 件の賞賛
返信

1,775件の閲覧回数
t2865k5
Contributor I

Dear NXP ,

I don't use uuu tool on my imx8mp board . I run command as follows:

./imx-make.sh bootloader kernel -j4 2>&1 | tee build-log.txt

 

I only update u-boot , kernel image and device tree to SD card (/dev/sdb) .

(1) Which images need to be updated to sd card ? How should I run command?
Ex:
u-boot : sudo dd if=imx-boot-imx8mpevk-sd.bin-flash_evk of=/dev/sdb bs=1k seek=32 conv=sync

kernel image : ?

kernel device tree: ?

 

 

0 件の賞賛
返信

1,781件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @t2865k5!

Thank you for contacting NXP Support!


You can use the uuu_imx_android_flash tool for that purpose.
 
Please check Table 2 of our Android Quick Start Guide for the options and examples of usage for iMX8MP.
 
https://www.nxp.com/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf

Best Regards!

Chavira

0 件の賞賛
返信