How to update QT 5.5 to QT5.8 on Yocto Project 2.4?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update QT 5.5 to QT5.8 on Yocto Project 2.4?

2,252件の閲覧回数
wangtsungli
Contributor IV

Hi community,

Before I used Yocto Project 2.4, I was working on Yocto Project 2.0 with QT 5.5 version.

However, while I change to Yocto Project 2.4 I find out that eglfs is not working on Yocto 2.4.

As this reason, I want to update QT version from 5.5 to 5.8 separately on Yocto 2.0 version.

How to do that?

Or there are any other suggestions?

Thanks in Advanced!

0 件の賞賛
返信
1 返信

1,820件の閲覧回数
turker
Contributor IV

You can go into meta-qt5 directory and switch to a branch that contains QT5.8 using git. I think pyro branch of meta-qt5 contains QT5.8. Though I am not sure if this is the correct approach. Switching to another branch may cause incompatibilities with existing layers or recipes.

0 件の賞賛
返信