How to turn on wifi in android oreo?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to turn on wifi in android oreo?

1,265件の閲覧回数
21300466
Contributor II

Hello, i succeed to boot my device(imx6dl) with android 8.0.

But i can't use wifi on my device. When i push wifi on button, it goes back to turn off state showing this error message "alloc_config_range: [hex num, hex num) PFNs busy.

What should i edit to make wifi work on my device?

Thanks in advance. 

ラベル(3)
1 返信

1,146件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello @ByeongHeon YOO

This error it is usually related to the MAC Address of the WIFI it is not configure or set,   try to add the MAC Address of your WIFI card, in the config file of the driver provided by the  Wifi Chip.   or try with a Ifconfig to set the MAC address before enable it.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------