How to turn on the MX6Q_SABRE-SDB by the RESET button

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to turn on the MX6Q_SABRE-SDB by the RESET button

跳至解决方案
1,310 次查看
yuuki
Senior Contributor II

Dear all,

We run AndroidKK4.4.3 on MX6Q_SABRE-SDB.

We want to boot the system by RESET button after it was turned off(shutdown) by POWER ON button.
In SABRE-SDB, the PWRON signal of RESET button(SW2) is connected to PWRON pin of PF0100.

In this case, we understood that the PWRON_CFG of PF0100 should be set to 1.
Is our understanding right?

In addition, is there the point that should be taken care of?

Best Regards,
Yuuki

标签 (2)
标记 (4)
0 项奖励
回复
1 解答
1,208 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

I think you are right, however in such case in original SDB

schematic wdog(software reset U507 on SPF-27392 p.21

i.MX6_SABRE_SDP_DESIGNFILES) will not work.

For turning ON board with button one can try to implement "optional"

U509 circuit.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,209 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

I think you are right, however in such case in original SDB

schematic wdog(software reset U507 on SPF-27392 p.21

i.MX6_SABRE_SDP_DESIGNFILES) will not work.

For turning ON board with button one can try to implement "optional"

U509 circuit.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复