Dear all,
We run AndroidKK4.4.3 on MX6Q_SABRE-SDB.
We want to boot the system by RESET button after it was turned off(shutdown) by POWER ON button.
In SABRE-SDB, the PWRON signal of RESET button(SW2) is connected to PWRON pin of PF0100.
In this case, we understood that the PWRON_CFG of PF0100 should be set to 1.
Is our understanding right?
In addition, is there the point that should be taken care of?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi Yuuki
I think you are right, however in such case in original SDB
schematic wdog(software reset U507 on SPF-27392 p.21
i.MX6_SABRE_SDP_DESIGNFILES) will not work.
For turning ON board with button one can try to implement "optional"
U509 circuit.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuuki
I think you are right, however in such case in original SDB
schematic wdog(software reset U507 on SPF-27392 p.21
i.MX6_SABRE_SDP_DESIGNFILES) will not work.
For turning ON board with button one can try to implement "optional"
U509 circuit.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------