How to transmit the packet for USB compliance tests for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to transmit the packet for USB compliance tests for i.MX6

Jump to solution
1,864 Views
yuuki
Senior Contributor II

Dear all,

We want to perform a USB compliance test for USB Host port of i.MX6.
It is necessary to transmit a test packet from USB Host port.

We think that USB Host must be entered into such mode.
Would you teach the register setting to transmit a test packet from USB Host port?

May I have advice?

Best Regards,
Yuuki

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

please check sect.34.9 "Testing the host mode"

iMX6_Firmware_Guide.pdf included in SDK

i.MX 6Series Platform SDK

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,527 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

please check sect.34.9 "Testing the host mode"

iMX6_Firmware_Guide.pdf included in SDK

i.MX 6Series Platform SDK

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply