How to test imx6s with IEEE 1149.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to test imx6s with IEEE 1149.1

1,483件の閲覧回数
zhengluyan
Contributor II
In the boundary scan test of imx6s motherboard, the correct idcode cannot be obtained. In addition to the standard JTAG 5 wires (JTAG)_ TMS、JTAG_ TCK、JTAG_ TRSTB、JTAG_ TDI、JTAG_ Does imx6s have special control when entering boundary scan mode? How to test imx6s with IEEE 1149.1.
0 件の賞賛
返信
5 返答(返信)

1,475件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Luyan

 

for boundary scan mode JTAG_MOD should be high, also one can look at

sect.Chapter 9  Using BSDL for Board-level Testing

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

 

Best regards
igor

1,452件の閲覧回数
zhengluyan
Contributor II

hello dear sir:

                     JTAG in e-fuse bits_ Smode [1:0] and SJC_ Does disable need to be 0?           

 

Thanks very much

0 件の賞賛
返信

1,424件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

1,407件の閲覧回数
zhengluyan
Contributor II

Hi~igorpadykov :

        I want to know what means"BSDL was only tested at 1.8 V." in the document IMX6DQ6SDLHDG.pdf

Thanks very much!

0 件の賞賛
返信

1,459件の閲覧回数
zhengluyan
Contributor II

hello dear sir:

       Below is the board settings which I have used:

       JTAG_MOD is High;

       POR_B is High;

      BOOT_MODE[1:0] is [1:0] or[0:0] ?

     What does "BSDL was only tested at 1.8 V." mean?  is NVCC_JTAG is 1.8V or all NVCC power is 1.8V? or  other ?

  Thanks very much

     

 

0 件の賞賛
返信