How to terminate unused CLK1_P/N on iMX8M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to terminate unused CLK1_P/N on iMX8M?

431 Views
fxsdes
Contributor I

On the iMX8M, does one need to terminate CLK1_P/N and CLK2_P/N when they are not used? 

The Dev Kit schematic shows 100 Ohm parallel termination resistors, but there is no mention of how best to handle these un-used signals in the Hardware Development Guide.

Labels (1)
0 Kudos
1 Reply

370 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Customer may leave them floating if not used.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos