How to support the TI's TLV320ADC6140 sound codec?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to support the TI's TLV320ADC6140 sound codec?

940 Views
chadA
Contributor III

Hi all,

Now I'm trying to replace the wm8960 with TI's TLV320ADC6140 to act as the codec for the sound card.

The base code is from TI: https://www.ti.com.cn/tool/cn/TLV320ADCX140SW-DRIVERS

And this code can't work directly, but I fixed it with the post of Nvidia: https://forums.developer.nvidia.com/t/tlv320adcx140-audio-adc-with-tx2/122311

Now the codec could register successfully.

But the sound card still not work, it needs the "mclk", and report "failed to get codec clk: -2" in imx-wm8960.c. And I am not sure how to fix this.

Anyone knows the issue?

Best regards~

Chad

Labels (1)
0 Kudos
Reply
4 Replies

880 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

There are no examples about how to support a dual codec configuration but should be similar to one codec configuration as separated sound cards with the respective device tree configuration and external connections.

Bets regards.

0 Kudos
Reply

914 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

Your TLV320ADCX140 seems to use the tlv320adcx140.c and tlv320adcx140.h source codes but your log is reporting an error in imx-wm8960.c file.

I suggest you take a look on this post

Best regards.

0 Kudos
Reply

903 Views
chadA
Contributor III

Dear @JorgeCas ,

Thanks for your reply.

Like I said before, now my codec driver should be fine, and this codec driver is based on TI.

But I still need a machine driver, like imx-wm8960.c.

And I am not sure how to implement this file for TLV320ADC6140. So I tried to connect the codec to the cpu via imx-wm8960.c.

Is this a good choice? Or maybe I should use eukrea-tlv320.c is better?

Thanks

Chad

 

0 Kudos
Reply

888 Views
chadA
Contributor III

Hi @JorgeCas

Now there are 2 codecs on my board, So I enabled the SAI1 and SAI2。

Then when I tried to config the route, How do I deal with CPU-Capture?

Thanks

Chad

0 Kudos
Reply