How to support MXIC nand flash?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to support MXIC nand flash?

跳至解决方案
3,297 次查看
9crkzhou
Contributor III

I'm using MX283

L2.3.35

default is not supporting MXIC

my new chip is MX30LF1G08AA  128M 1024blocks  128k per block  64pages per block

to support MFGTOOL

I need a updater.sb file

then I built the LTIB and get a new updater_ivt.sb and updater.sb

mainly modiffied those place:

driver/mtd/nand/nand_ids.c

add

{"NAND 238MiB 3,3V 8-bit", 0xF0, 0,128,0,LP_OPTIONS},

add

{0xc2, "Macronix"},

driver/mtd/nand/nand_device_info.c

add

  {

    .end_of_table             = false,

    .manufacturer_code        = 0xc2,

    .device_code              = 0xf1,

    .cell_technology          = NAND_DEVICE_CELL_TECH_SLC,

    .chip_size_in_bytes       = 128LL*SZ_1M,

    .block_size_in_pages      = 64,

    .page_total_size_in_bytes = 2*SZ_1K,

    .ecc_strength_in_bits     = 4,

    .ecc_size_in_bytes        = 512,

    .data_setup_in_ns         = 30,

    .data_hold_in_ns          = 20,

    .address_setup_in_ns      = 0,

    .gpmi_sample_delay_in_ns  = 6,

    .tREA_in_ns               = -1,

    .tRLOH_in_ns              = -1,

    .tRHOH_in_ns              = -1,

    "Macronix",

    },

it not work!

how to deal with this?

标签 (2)
标记 (2)
1 解答
2,509 次查看
9crkzhou
Contributor III

fix already.

only need to modify nand_ids.c and nand_device_info.c

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,510 次查看
9crkzhou
Contributor III

fix already.

only need to modify nand_ids.c and nand_device_info.c

0 项奖励
回复
2,509 次查看
MarekVasut
Senior Contributor I

If possibly , try using mainline U-Boot 2014.01 and mainline Linux at least 3.10.xx . They have myriad of fixes .