How to support 8bit serial RGB LCD with 6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to support 8bit serial RGB LCD with 6ULL

2,433 Views
stoneliu
Contributor II

Hi Team,

Please give some comments how to support 8bit serial RGB LCD, attached file is the LCD spec.

Before this LCD worked well for i.MX257, now we are porting this to 6ULL. We tried in DOTCLK interface 3 weeks, but still can't resolve. 

Configed as below, but can't work. Please help, this is very urgent for us.

LCD_DATABUS_WIDTH  8bits

WORD_LENGTH   24 bits

Thanks,

Stone

Labels (2)
0 Kudos
Reply
3 Replies

1,969 Views
Jeffye
Contributor I

elcdif does not support serial 8 bit initial timing setting
You need to modify the elcdif register by yourself, the example is as follows

base->VDCTRL2 =
((uint32_t)config->hsw << LCDIF_VDCTRL2_HSYNC_PULSE_WIDTH_SHIFT) |
(((uint32_t)config->hfp + (uint32_t)config->hbp + (uint32_t)config->panelWidth * 3 + (uint32_t)config->hsw))
<< LCDIF_VDCTRL2_HSYNC_PERIOD_SHIFT;


base->VDCTRL4 = LCDIF_VDCTRL4_SYNC_SIGNALS_ON_MASK |
(((uint32_t)config->panelWidth * 3) << LCDIF_VDCTRL4_DOTCLK_H_VALID_DATA_CNT_SHIFT);

0 Kudos
Reply

2,416 Views
zhenhua_lin
Contributor I

Hi, 

I check the uboot source code on version uboot-imx_v2018.03.

The mxsfb.c init lcd function mxs_lcd_init write as bellow:

{{{

static void mxs_lcd_init(GraphicDevice *panel,
struct ctfb_res_modes *mode, int bpp)
{
struct mxs_lcdif_regs *regs = (struct mxs_lcdif_regs *)(ulong)(panel->isaBase);
uint32_t word_len = 0, bus_width = 0;
uint8_t valid_data = 0;

/* Kick in the LCDIF clock */
mxs_set_lcdclk(panel->isaBase, PS2KHZ(mode->pixclock));

/* Restart the LCDIF block */
mxs_reset_block(&regs->hw_lcdif_ctrl_reg);

switch (bpp) {
case 24:
word_len = LCDIF_CTRL_WORD_LENGTH_24BIT;
bus_width = LCDIF_CTRL_LCD_DATABUS_WIDTH_24BIT;
valid_data = 0x7;
break;
case 18:
word_len = LCDIF_CTRL_WORD_LENGTH_24BIT;
bus_width = LCDIF_CTRL_LCD_DATABUS_WIDTH_18BIT;
valid_data = 0x7;
break;
case 16:
word_len = LCDIF_CTRL_WORD_LENGTH_16BIT;
bus_width = LCDIF_CTRL_LCD_DATABUS_WIDTH_16BIT;
valid_data = 0xf;
break;
case 8:
word_len = LCDIF_CTRL_WORD_LENGTH_8BIT;
bus_width = LCDIF_CTRL_LCD_DATABUS_WIDTH_8BIT;
valid_data = 0xf;
break;
}

writel(bus_width | word_len | LCDIF_CTRL_DOTCLK_MODE |
LCDIF_CTRL_BYPASS_COUNT | LCDIF_CTRL_LCDIF_MASTER,
&regs->hw_lcdif_ctrl);

writel(valid_data << LCDIF_CTRL1_BYTE_PACKING_FORMAT_OFFSET,
&regs->hw_lcdif_ctrl1);

#ifdef CONFIG_IMX_MIPI_DSI_BRIDGE
writel(LCDIF_CTRL2_OUTSTANDING_REQS_REQ_16, &regs->hw_lcdif_ctrl2);
#endif

writel((mode->yres << LCDIF_TRANSFER_COUNT_V_COUNT_OFFSET) | mode->xres,
&regs->hw_lcdif_transfer_count);

#ifdef CONFIG_IMX_SEC_MIPI_DSI
writel(LCDIF_VDCTRL0_ENABLE_PRESENT |
LCDIF_VDCTRL0_VSYNC_PERIOD_UNIT |
LCDIF_VDCTRL0_VSYNC_PULSE_WIDTH_UNIT |
mode->vsync_len, &regs->hw_lcdif_vdctrl0);
#else
writel(LCDIF_VDCTRL0_ENABLE_PRESENT | LCDIF_VDCTRL0_ENABLE_POL |
LCDIF_VDCTRL0_VSYNC_PERIOD_UNIT |
LCDIF_VDCTRL0_VSYNC_PULSE_WIDTH_UNIT |
mode->vsync_len, &regs->hw_lcdif_vdctrl0);
#endif
writel(mode->upper_margin + mode->lower_margin +
mode->vsync_len + mode->yres,
&regs->hw_lcdif_vdctrl1);
writel((mode->hsync_len << LCDIF_VDCTRL2_HSYNC_PULSE_WIDTH_OFFSET) |
(mode->left_margin + mode->right_margin +
mode->hsync_len + mode->xres),
&regs->hw_lcdif_vdctrl2);
writel(((mode->left_margin + mode->hsync_len) <<
LCDIF_VDCTRL3_HORIZONTAL_WAIT_CNT_OFFSET) |
(mode->upper_margin + mode->vsync_len),
&regs->hw_lcdif_vdctrl3);
writel((0 << LCDIF_VDCTRL4_DOTCLK_DLY_SEL_OFFSET) | mode->xres,
&regs->hw_lcdif_vdctrl4);

writel(panel->frameAdrs, &regs->hw_lcdif_cur_buf);
writel(panel->frameAdrs, &regs->hw_lcdif_next_buf);

/* Flush FIFO first */
writel(LCDIF_CTRL1_FIFO_CLEAR, &regs->hw_lcdif_ctrl1_set);

#ifndef CONFIG_VIDEO_MXS_MODE_SYSTEM
/* Sync signals ON */
setbits_le32(&regs->hw_lcdif_vdctrl4, LCDIF_VDCTRL4_SYNC_SIGNALS_ON);
#endif

/* FIFO cleared */
writel(LCDIF_CTRL1_FIFO_CLEAR, &regs->hw_lcdif_ctrl1_clr);

/* RUN! */
writel(LCDIF_CTRL_RUN, &regs->hw_lcdif_ctrl_set);
}

}}}

That can not use 8bits bus-width interface to 24 bits LCD. Please ref the case session.

Thanks.

Zhenhua

0 Kudos
Reply

2,422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stone

 

one can look at below link with similar issue:

https://community.nxp.com/t5/i-MX-Processors/LCDIF-8bits-bus-width-interface-to-24-bits-LCD-display-...

 

Best regards
igor

0 Kudos
Reply