hello,
If the answer below is correct,
is Dumb PMIC enabled even if DP_EN in SNVS_LP Control Register is not set to "1"?
Is the TOP value valid even if DP_EN is not set to "1"?
Answer excerpt
i.MX7D supports only dumb mode, also there are no options to reconfigure behavior of PMIC_ON_REQ signal.
best regards
Goto