Dear all,
I came cross a problem about adb.
the problem:
root@sabresd_6dq:/ # adb logcat
* daemon not running. starting it now on port 5038 *
ehci_fsl_bus_resume begins, Host 1
* daemon started successfully *
ehci_fsl_bus_resume ends, Host 1
- waiting for device -
and
root@sabresd_6dq:/system/app # adb install myserial.apk
* daemon not running. starting it now on port 5038 *
ehci_fsl_bus_resume begins, Host 1
* daemon started successfully *
ehci_fsl_bus_resume ends, Host 1
error: device not found
- waiting for device -
how to solve the problem? Thanks !
Hello !
Please try solution from the following thread :
i.MX6DL Driver and Getting Windows 7 To Communicate As An Android Device
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,where I can find the android_usb_fsl.zip?
now,my IMX6Q-SDB has not a screen,IIcan only operate it through the console.so how should I do?
Is the ADB working ?
"The versions later than Android JB 4.2.2 introduce public key authentication
policy when connecting to PC host via ADB. This feature will keep ADB offline
until the device and PC pass authentication."
Please refer to "Android_Frequently_Asked_Questions.pdf" in FSL Android documentation.
Regards,
Yuri.
Hello,whether we can set the USB debugging method throght command line ?if can ,what command can be use ?
Thank you !
hello, because my board hasn't lcd screen ,then whether the following step can't operate?
5. Enable the "USB debugging" option on the i.MX6 device
System settings -> Developer options -> USB debugging