How to setting up ENET2_TX_CLK pin in DTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to setting up ENET2_TX_CLK pin in DTS

946 Views
liangfeng_0824
Contributor I

I am using ENET2_TX_CLK as USB OTG2_ID now.

What is the value of MX6UL_PAD_ENET2_TX_CLK__ANATOP_OTG2_ID in device tree system?

pinctrl_usbotg2: usbotg2grp {

fsl,pins = < MX6UL_PAD_ENET2_TX_CLK__ANATOP_OTG2_ID      ?value?

        >;

};

Labels (1)
0 Kudos
Reply
4 Replies

815 Views
igorpadykov
NXP Employee
NXP Employee

Hi liangfeng_0824

one can set it to the same value as for *ANATOP_OTG1_ID in example on

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-ddr3-arm2.d...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

815 Views
liangfeng_0824
Contributor I

What is the difference between imx6ul-14*14-evk  board hardware and imx6ul-14*14-ddr3-arm2 hardward ?  

0 Kudos
Reply

815 Views
igorpadykov
NXP Employee
NXP Employee

imx6ul-14*14-ddr3-arm2 is internal validation board, imx6ul-14*14-evk  board

was developed for customers use.

Best regards
igor

0 Kudos
Reply

815 Views
liangfeng_0824
Contributor I

i use imx6ul platform ;   Can you reply me as soon as possible?

0 Kudos
Reply