Hi NXP,
My imx processor is "iMX8M Plus", I want to setting in M7.
When I finish setting, I can't probe any signal from MDC/MDIO.
My setting as follows,
1. gpio setting
- {pin_num: AH28, peripheral: ENET_QOS, signal: enet_qos_mdc, pin_signal: ENET_MDC, PUE: Weak_Pull_Down, ODE: Open_Drain_Disable, FSEL: Slow, DSE: X6, SION: DISABLED}
- {pin_num: AH29, peripheral: ENET_QOS, signal: enet_qos_mdio, pin_signal: ENET_MDIO, PE: Enabled, HYS: CMOS, PUE: Weak_Pull_Down, ODE: Open_Drain_Disable, FSEL: Slow,
DSE: X6, SION: DISABLED}
2. other setting
#define EXAMPLE_ENET ENET1
#define EXAMPLE_CLOCK_FREQ \
(CLOCK_GetPllFreq(kCLOCK_SystemPll1Ctrl) / (CLOCK_GetRootPreDivider(kCLOCK_RootEnetQos)) / \
(CLOCK_GetRootPostDivider(kCLOCK_RootEnetQos)))
- BOARD_InitModuleClock
CLOCK_SetRootMux(kCLOCK_RootEnetQos, kCLOCK_EnetQosRootmuxSysPll1Div5);
CLOCK_SetRootDivider(kCLOCK_RootEnetQos, 1U, 10U);
Thanks.
Best Regards,
Wayne.