How to set vsync-len for MIPI-DSI Host?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set vsync-len for MIPI-DSI Host?

3,897 次查看
huynhduchau
Contributor I

Hello all

Does anyone know how to set DSI vsync-len value on IMX8MQ?

I've looked at chapter 13.6 in IMX8MQ Reference Manual (IMX8MDQLQRM), it seems only hsync-len can be set by  MIPI_DSI_HOST_DPI_INTFC_DSI_HOST_CFG_DPI_HSA register.

However, these MIPI-DSI parameters (hsync len, vsync len) can be found in IMX8MM reference manual ( 13.5.5.1.13). 

Thanks!

0 项奖励
回复
3 回复数

3,723 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can set this in the dts file, for example:rm67191 

  display-timings {
   timing {
    clock-frequency = <132000000>;
    hactive = <1080>;
    vactive = <1920>;
    hfront-porch = <20>;
    hsync-len = <2>;
    hback-porch = <34>;
    vfront-porch = <10>;
    vsync-len = <5>;
    vback-porch = <4>;
    hsync-active = <0>;
    vsync-active = <0>;
    de-active = <0>;
    pixelclk-active = <0>;
   };
  };

0 项奖励
回复

3,723 次查看
huynhduchau
Contributor I

Thanks for hint.

But I believe vsync-len value won't be set to MIPI-DSI bridge.

Kernel driver lacks of setting vsync-len as I read from this code:

static void nwl_dsi_config_dpi(struct nwl_mipi_dsi *dsi)
{
struct device *dev = dsi->dev;
struct mipi_dsi_device *dsi_device = dsi->dsi_device;
struct videomode vm;
enum dpi_pixel_format pixel_format =
nwl_dsi_get_dpi_pixel_format(dsi_device->format);
enum dpi_interface_color_coding color_coding =
nwl_dsi_get_dpi_interface_color_coding(dsi_device->format);
bool burst_mode;

drm_display_mode_to_videomode(dsi->curr_mode, &vm);

nwl_dsi_write(dsi, INTERFACE_COLOR_CODING, color_coding);
nwl_dsi_write(dsi, PIXEL_FORMAT, pixel_format);
DRM_DEV_DEBUG_DRIVER(dev, "DSI format is: %d (CC=%d, PF=%d)\n",
dsi_device->format, color_coding, pixel_format);

/*TODO: need to make polarity configurable */
nwl_dsi_write(dsi, VSYNC_POLARITY, 0x00);
nwl_dsi_write(dsi, HSYNC_POLARITY, 0x00);

burst_mode = (dsi_device->mode_flags & MIPI_DSI_MODE_VIDEO_BURST) &&
!(dsi_device->mode_flags & MIPI_DSI_MODE_VIDEO_SYNC_PULSE);

if (burst_mode) {
nwl_dsi_write(dsi, VIDEO_MODE, 0x2);
nwl_dsi_write(dsi, PIXEL_FIFO_SEND_LEVEL, 256);
} else {
nwl_dsi_write(dsi, VIDEO_MODE, 0x0);
nwl_dsi_write(dsi, PIXEL_FIFO_SEND_LEVEL, vm.hactive);
}

nwl_dsi_write(dsi, HFP, vm.hfront_porch);
nwl_dsi_write(dsi, HBP, vm.hback_porch);
nwl_dsi_write(dsi, HSA, vm.hsync_len);

nwl_dsi_write(dsi, ENABLE_MULT_PKTS, 0x0);
nwl_dsi_write(dsi, BLLP_MODE, 0x1);
nwl_dsi_write(dsi, ENABLE_MULT_PKTS, 0x0);
nwl_dsi_write(dsi, USE_NULL_PKT_BLLP, 0x0);
nwl_dsi_write(dsi, VC, 0x0);

nwl_dsi_write(dsi, PIXEL_PAYLOAD_SIZE, vm.hactive);
nwl_dsi_write(dsi, VACTIVE, vm.vactive);
nwl_dsi_write(dsi, VBP, vm.vback_porch);
nwl_dsi_write(dsi, VFP, vm.vfront_porch);
}

Btw, I'm using LCDIF as source for the bridge, and LCDIF register values seem correct.

0 项奖励
回复

3,723 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, dsi bridge doesn't set this in the dts file, depends on what panel you use, you can add this in the dts file according to the panel you use

0 项奖励
回复