How to set to make imx6q HDMI display full screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set to make imx6q HDMI display full screen

1,991件の閲覧回数
zjz
Contributor II

the left margin and right margin of picture the imx6q HDMI(1920x1080) display on TV is too wide.

Here is fb_videomode when resolution is 1920x1080

mxc_cea_mode[16] = {
NULL, 60, 1920, 1080, 6734, 148, 88, 36, 4, 44, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
}

I changed the value of left margin and right margin showed above

The value is writen to corresponding register in function hdmi_av_composer but nothing changed. 

so  how can I eliminate the left and right margin imx6q HDMI display on TV?

ラベル(1)
タグ(2)
3 返答(返信)

1,613件の閲覧回数
jamiew
Contributor III

Also worth double checking your TV is set to "Just Scan" in the aspect ratio menu rather than "16:9" etc as TVs often don't map 1920x1080 pixel to pixel.

0 件の賞賛
返信

1,613件の閲覧回数
zjz
Contributor II

Thks for your reply

0 件の賞賛
返信

1,613件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you are using Android and you have cloned displays (for example, LVDS display and HDMI monitor), both will be set to the lower resolution (typically, the LVDS display resolution) although manually setting the resolution on the FB driver. If you want full screen on the HDMI screen, you could try disabling the LVDS display and only sending the video to the HDMI interface. If you want to force the resolution, you could try using ADB commands for manually changing it on this way.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------