How to set the fdt_file value on yocto project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set the fdt_file value on yocto project

1,773 Views
ChChang
Contributor II

Hi

My platform is i.mx8qm-mek, and the BSP is Linux L6.1.55_2.2.0.
Currently, the generated image file uses
imx8qm-mek-rpmsg.dtb as the fdt_file for uboot.
I would like to change the default value of
fdt_file to imx8qm-mek-hdmi.dtb before Yocto generates the image, without manually setting it in uboot.
Which conf file should I modify?
Thanks!

CH

0 Kudos
Reply
2 Replies

1,727 Views
Harvey021
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,723 Views
ChChang
Contributor II

Thanks for your reply ,
This problem was solved, thanks a lot!

Regards,

CH

0 Kudos
Reply