How to set the SDRAM EXTENDED MODE REGISTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set the SDRAM EXTENDED MODE REGISTER

1,108 Views
daisukeyoshinar
Contributor II

Hello.

I'm using a custom board with i.MX RT1062.

I want to change the EXTENDED MODE REGISTER of SDRAM.
Reference Manual (IMXRT1060RM Rev. 2, 12/2019 Figure 25-5. IP command - SDRAM MODE REGISTER SET)
States that Address and BA are "VALUE".

I also found a change in MODE REGISTER settings using SEMC_SendIPCommand () in the SDK.

Is it possible to set EXTENDED MODE REGISTER in the same way as MODE REGISTER ?
Where can I find the description of the correspondence between BA0, BA1 and VALUE ?

Best regards,
Daisuke Yoshinari

0 Kudos
Reply
1 Reply

1,100 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to set EXTENDED MODE REGISTER in the same way as MODE REGISTER ?
-- Yes, I think so.
2) Where can I find the description of the correspondence between BA0, BA1 and VALUE ?
-- I think you need to refer to the datasheet of the SDRAM.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply