I'm using an imx6slevk board with yocto bsp and I've loaded the g_cdc module to use the usb port as serial port and as ethernet.
I'm using ifconfig usb0 192.168.44.30 netmask 255.255.255.0 to set the ip address of the usb port of the target
(as mentioned here: Using the USB port (as device) )
I'd like to do this automatically every time the board boots instead of having to type it every time.
I followed this thread https://community.nxp.com/thread/459867 but setting in u-boot doesn't seem to have an effect on usb's ip address. what changes should I make in the source to do this?
解決済! 解決策の投稿を見る。
You can add "ifconfig usb0 192.168.44.30 netmask 255.255.255.0" into startup script.
That worked for me
Just added a script in /etc/profile.d
Thanks for the info