How to set imx7d eim bus clock frequency?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set imx7d eim bus clock frequency?

1,525 次查看
864535720
Contributor II

Hello everyone
my development board is IMX7DSABRE. Linux kernel version is 4.9.88
When I use the EIM bus to communicate with the FPGA, I use asynchronous 16-bit data lines and 27 address lines for communication. After reading the manual, I found that the asynchronous access method does not require the EIM_BCLK clock. But I also saw the description of EIM clk cycle in the IMX7DRM manual. For example, EIM_CSnGCR2 [7-4] -DAPS: 0010 5 EIM clk cycles between start of access and first DTACK check etc.
Question 1: I want to know what is the EIM clk cycles here? According to which register is it configured?

Question 2: I measured the clock frequency of my EIM_BCLK to be 120MHz. I changed the value of the BCD field of the EIM_CSnGCR1 register. I went to measure and found that it was still 120MHz. Why is this?

My EIM register configuration is as follows:
Register:    CSxGCR1 CSxGCR2    CSxRCR1    CSxRCR2     CSxWCR1 CSxWCR2
Address:  0x30bc0000 0x30bc0004 0x30bc0008 0x30bc000c 0x30bc0010 0x30bc0014
Value:      0x00613081 0x00000001 0x1c022000 0x0000c000 0x1404a38e 0x00000000

标签 (3)
0 项奖励
回复
1 回复

1,473 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 其东 刘 

one can try to debug it using weim driver sources:

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

imx7d.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

imx-weim.c\bus\drivers - linux-imx - i.MX Linux kernel 

Description in sect,3.2 EIM NOR attached Linux Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复