Hi community,
I want to confirm how to set i.MX6 FCB values for NAND.
Please see Table 8-12 in IMX6SDLRM (Rev.1) and my questions as below.
[Q1]
At first I want to confirm whether FCB is unique data for i.MX series or not.
Could you let me know it?
[Q2]
The unit of m_NandTiming values are "nano seconds" as per NAND datasheet.
So I should program "0x0A" to m_NandTiming if the correspondent value in NAND datasheet is "10 ns".
Is my understanding correct?
[Q3]
As per NAND datasheet, REA, RLOH, and RHOH values are written as max value.
Should I program the max values to m_NnandTiming[7:5]?
[Q4]
I want to confirm what is "dsample_time" and "nand_timing_state".
What parameters in NAND datasheet are corresponded them?
[Q5]
To disable "Onfi_sync_enable", should I set it to 0x00000000?
Best Regards,
Satoshi Shimoda