I need a set of environment variables to be available in the shell after booting the custom image from the target hardware.
1. Can I set these variables using any patch from bitbake itself?
1.a. If yes, please let me know what are the modifications to be done.
1.b. If no, please let me know the alternative way to achieve this.
2. How can I achieve enhancement in compositor performance for the following Yocto configuration?
Yocto version: 4.1.15-2.0.0
Target hardware: i.MX6Q
3. Also, need some details in understanding the following patch files.
0008-MGS-1668-xwld-System-can-not-boot-up-to-desktop.patch
0009-MGS-1284-xwld-Re-implement-weston-2d-renderer-with-p.patch
0010-MGS-1284-1-xwld-Re-implement-weston-2d-renderer-with.patch
0011-MGS-1724-xwld-G2D-compositor-build-failed-in-slevk-b.patch
0012-MGS-1783-xwld-Add-clone-mode-support-for-multi-displ.patch
0013-MGS-1945-Use-common-API-to-support-G2d-compositor.patch
0014-MGS-1987-Get-stride-from-the-FB-buffe.patch
Thanks in advance. :smileyhappy: