Hi, I have a question about how to change a PCIe device's memory address on i.MX6.
Now, I have a PCIe EP device connected to i.MX6 Quad (running Linux 3.14.52) and issuing lspci command shows the following values for the device:
Memory at 01100000 (32-bit, non-prefetchable) [size=1M]
Memory at 01200000 (32-bit, non-prefetchable) [size=1M]
The question is how can I change these values (01100000/01200000)?
Should I modify device tree or Linux kernel's source code?
Regards,
已解决! 转到解答。
Hi t_kuha
please check PCI EP examples (0001-ENGR00268112-pcie-emaluate-the-pcie-ep-as-ram-device.patch.zip) on
i.MX6Q PCIe EP/RC Validation System
for latest kernels one can look at sect.40.4 Using PCIe Endpoint and Running Tests attached Linux Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi t_kuha
please check PCI EP examples (0001-ENGR00268112-pcie-emaluate-the-pcie-ep-as-ram-device.patch.zip) on
i.MX6Q PCIe EP/RC Validation System
for latest kernels one can look at sect.40.4 Using PCIe Endpoint and Running Tests attached Linux Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------